Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 177

Sort:
How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

Comparisons of GNSS Solutions
View this table for product comparisons.

FAQ 2014-03-25

How can I source a pulsed signal on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-09-16

How do you clear the M9381A PXIe Vector Signal Generator and M9380A PXIe CW Source modules memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2013-08-06

How do I change the 10 MHz reference source if Signal Studio for pulse building doesn’t detect the reference?
Most of the time, Signal Studio will recognize the reference; however, it can be changed in the download -> customize menu.

FAQ 2013-05-16

Is there a way to put insert a missing pulse into the signal?
Yes, you can add a “Off time” object to the pulse pattern and change the duration to meet your pulse requirements.

FAQ 2013-05-16

Are there any options to adjust the pulse definitions within Signal Studio for pulse building?
No, at the moment the rise and fall times are defined by their 0-100 percent points and the pulse width is defined to be the 100-100 percent point.

FAQ 2013-05-16

What USB storage devices are compatible with the MXG?
The MXG is now compatible with most USB storage devices.

FAQ 2013-03-13

Do User channel corrections cover multiple attenuator steps?
Yes. Bypass step, 0 dB step, and 5 dB step.

FAQ 2013-02-26

When I use the 30-day trial license of the Signal Studio for WiMAX™, how can I check the number of days remaining on temporary license?
Press the front panel keys: Utility > Instrument Adjustments > Instrument Options > Waveform Licenses

FAQ 2013-01-28

66xxA, E363xA and E364xA: Ca Keysight Power Supplies Sink Current?
Yes! Sinking, or down-programming, is the ability to pull current into the positive terminal of a power supply.

FAQ 2013-01-22

Does the Signal Studio for Pulse Building software run on a National Instruments embedded PXI controller like the one that comes with the N6030A?
Yes, it does. However, the Keysight I/O Libraries may need to be installed as a secondary VISA and then the NI Tulip DLL may need to be enabled.

FAQ 2012-12-30

Is there a way to simulate jitter in my pulse pattern?
Yes, Signal Studio for pulse building allows you to add jitter on the pulse width and pulse repetition interval.

FAQ 2012-12-30

On my E8267D, I get an error that the signal requires more repeats than supported, can I increase this limit with the internal baseband option?
No. To increase the number of pulse capacity either upgrade to an External Baseband option with the N8241A AWG or ...

FAQ 2012-12-30

Is there an easy way to save a pulse pattern and send it to another person?
Yes, simply save the entire .pbp or you can export the pattern using the “export pattern” function.

FAQ 2012-12-30

When would I use ALC Hold?
ALC Hold is used for pulses with rise and fall times greater than 100 ns. It is used with pulses that do not have constant envelope modulation (such as AM Step), and with multiple pulses where the pulses have different amplitudes.

FAQ 2012-12-30

Can I turn off the N6030A arbitrary waveform generator predistortion from the N7620B Signal Studio for Pulse Building to get more power?
No. The N7620B software does not allow the N6030A predistortion to be turned off.

FAQ 2012-12-30

How can I get 1 GHz modulation bandwidth below 3.2 GHz?
There is a special option that down converts the wideband signal. It is: E8267D Option H1S PSG with 1 GHz out for use by the Z5623AK92 down converter, 500 MHz – 3.2 GHz.

FAQ 2012-12-28

What happens when I turn the N6030A arbitrary waveform generator off?
You will probably need to reboot PC if you are using an MXI to PXI interface. All signal data is lost.

FAQ 2012-12-28

Why should I use Amplitude Offset?
Use the Amplitude Offset feature to account for any external gain or loss that is greater than 10 dB.

FAQ 2012-12-28

Why do I want to mirror the spectrum?
Mirror Spectrum reverses the spectrum of the waveform when it is downloaded. This is useful for systems with external upconversion and downconversion where the signal spectrum is mirrored by the conversion process.

FAQ 2012-12-28

What is the performance difference between the N8212A module with Option 016 and the N8241A arbitrary waveform generator synthetic instrument module?
The N8212A with Option 016 is based on the E8267D PSG signal generator with Option 016; the N8241A is based on the N6030A arbitrary waveform generator.

FAQ 2012-12-28

1 2 3 4 5 6 7 8 Next