Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 756

Упорядочить:
Why does my paralleled master/slave N8900 units display “UNR”?
The N8900 slave units can be unregulated (UNR) during certain conditions, so this display could be normal.

FAQ 2020-07-28

PDF PDF 10.01 MB
30 Day Free Trial Licenses for the M8000 Series
Overview of & links to all trial licenses within the M8000 product family.

FAQ 2020-07-17

Signal Generator Firmware Update Center
Download signal generator firmware, release notes, upgrade guide and FAQs.

FAQ 2020-06-19

What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2020-05-22

How do I upgrade my N5172B EXG Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2019-10-21

How do I upgrade my N5182B MXG Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2019-10-21

How do I find the HOST ID of my instrument or PC?
Keysight software options are licensed to many different types of hardware, using a unique hardware identifier called the Host ID. The Host ID is composed of 1, 2, or 3 elements, depending upon the software model and the target hardware platform.

FAQ 2019-07-10

How do I upgrade my N5166B CXG Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2019-04-26

Why is readback voltage/current different from actual value when the recall function is used after power cycling the unit?
Users may encounter incorrect voltage/current readback reading under the following conditions

FAQ 2019-02-27

Signal Generator (Signal Source) Upgrade Center
Information to perform a signal generator upgrade or signal source upgrade.

FAQ 2018-06-19

How Do I Measure the Bit Error Rate (BER) to a Given Confidence Level on the J-BERT M8020A and the M8040A High-Performance BERT?
How do I measure Bit Error Rate (BER) to a given confidence level on J-BERT M8020A and M8040A high-performance BERT?

FAQ 2018-03-01

M8020AU Upgrades for J-BERT M8020A high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option

FAQ 2017-12-13

Signal Analyzer LabVIEW Instrument Drivers
Supported models: N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, N8973B, N8974B, N8975B, N8976B, M8920A

FAQ 2017-12-01

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Save Time with a Modern Bench Power Supply
The new low cost DC Bench Power Supply from Keysight has three independent outputs & built in data logger. See how a modern Bench Power Supply can help you.

FAQ 2017-06-20

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

Firmware update error with "Cannot Open another Window"
I cannot update the firmware with the error message; "Cannot Open another Window"

FAQ 2016-08-04

How do I clear the External Reference Warning on the display?
Step by step procedure can be found here...

FAQ 2016-01-08

How do I set the reference to external, have notification of any external reference problems, and have it remain external with a Preset?
Process steps included here...

FAQ 2016-01-08

1 2 3 4 5 6 7 8 9 10 ... Следующие