Support technique
Mesure Electronique
Affiner la liste
Par industrie/technologie
Par type de contenu
- Document Library
- Démos
- Démonstration de base (110)
- Vidéos pratiques (1)
Par catégorie de produit
- Démos
1-25 sur 111
Kandou Bus and Keysight collaborate on an innovative test solution for chord signaling applications
Démonstration de base 2019-09-16 |
|
Keysight PCIe 3.0 and 4.0 Receiver Test Solution Link Equalization Test Setup
Get a quick overview of Keysight’s PCI Express test solution including the highly integrated Keysight J-BERT M8020A and the Keysight Infiniium V-Series oscillocope.
Démonstration de base 2017-08-17 |
|
Social/Viral video – social video
Musical tastes keep on changing, and so does technology. Today, it’s time to power up with the colorful new E36300A Series.
Démonstration de base 2017-07-25 |
|
Data log with your bench power supply, Keysight E36300 Series
Typically most test applications involve powering up a DUT with a power supply and taking measurements from it with an external data logger - you’ll need just ONE instrument to do both of those functions with the E36300 Triple Output Bench Power Supply.
Démonstration de base 2017-07-12 |
|
Bench Power Supply low range current mode, Keysight E36300 Series
Typically, different external shunts are required to measure low or high range current. In order to make testing more convenient to user, we have developed the E36300 Triple Output Bench Power Supply that is capable of sourcing and sensing both low and high range current. Let’s see how this works through a quick demonstration via battery charging.
Démonstration de base 2017-07-05 |
|
Bench Power Supply Auto Series/Parallel connections, Keysight E36300 Series
Bench Power Supply Auto Series/Parallel connections, Keysight E36300 Series
Démonstration de base 2017-06-29 |
|
Making Field Effect Transistor Characterization using SMU - Demo Guide
This B2900A demo guide shows how easily you can undertake FET characterization using the B2900A SMU step by step.
Démonstration de base 2017-06-19 |
![]() |
Triple Output Bench Power Supply Teardown, Keysight E36300 Series
Learn how the E36300 Triple Output Bench Power Supply was designed for the highest reliability and quiet operation. The linear design and ample filtering create low noise on the output. Each output is completely independent and can be connected in parallel or serial to provide higher current or voltage. Internal relays simplify the setup of auto-parallel and auto-series modes. Relays are also used to switch between 2 and 4 wire measurements. The Bench Power supply is built around a single processor which provides fast response to the front panel and over the USB and LAN interface.
Démonstration de base 2017-06-18 |
|
Making Time Domain Measurement with Continuous Source Using SMU - Demo Guide
This B2900A demo guide shows how easily you can make a time domain measurement with sourcing continuous current or voltage using the B2900A Series SMU step by step.
Démonstration de base 2017-06-06 |
![]() |
Making Time Domain Measurement with Staircase Source Using SMU - Demo Guide
This B2900A demo guide shows how easily you can make a time domain measurement with sourcing staircase current or voltage using the B2900A Series SMU step by step.
Démonstration de base 2017-06-05 |
![]() |
Making Time Domain Measurement with Pulsed Source Using SMU- Demo Guide
This B2900A demo guide shows how easily you can make a time domain measurement with sourcing pulsed current or voltage using the B2900A Series SMU step by step.
Démonstration de base 2017-06-03 |
![]() |
E36300 Triple Output Bench Power Supply Product Overview
The E36300 Bench Power Supply is designed to replace the E3631A Triple Output Power Supply. On the bench, the E36300 series power supply is ready for your application. With low output ripple/noise, large graphical display, accurate measurements of a wide range of currents and voltage you can test with confidence. The E36300 Bench Power Supply family has three models; E36311A 80W model with USB only, E36312A 80W model with LAN & USB, and the E36313A 160W model with twice the output current, LAN and USB.
Démonstration de base 2017-06-01 |
Langues
|
Using an External Trigger to Generate Pulses with the B2960A – Demo Guide
This B2960A demo guide shows how easily you can configure the B2960A Series to make it source pulses whenever it receives an external trigger signal step by step.
Démonstration de base 2017-05-30 |
![]() |
5G mmWave for Wideband Applications Demo - video
This video demonstration by Keysight 5G expert Greg Jue shows a 73GHz demo with 2GHz of modulation bandwidth for 5G mmWave applications.
Démonstration de base 2017-05-22 |
|
UXG Signal Generator Demo Videos on YouTube
Explore YouTube for videos of the N5193A UXG agile signal generator.
Démonstration de base 2017-03-27 |
|
Making Bipolar Transistor Characterization using SMU - Demo Guide
This B2900A demo guide shows how easily you can undertake BJT characterization using the B2900A SMU step by step.
Démonstration de base 2017-01-23 |
![]() |
N4917B Optical Receiver Stress Test Solution – Video
This video provides an overview about Keysight’s automated 100G optical receiver stress test solution N4917B. See why Keysight’s N4917B solution can help to significantly speed up the LR4, ER4 and SR4 optical receiver compliance test for 100G.
Démonstration de base 2016-11-30 |
|
Video: How to test coherent digital signal processors by generating impairments
This video covers how to test coherent digital signal processors. Through using an arbitrary waveform generator, together with optical modulation generation software, the video shows how to generate waveforms in real-time and change the properties of the signals generated at run-time to test coherent DSPs.
Démonstration de base 2016-11-30 |
|
How to characterize PAM-4 transmitters
This video will illustrate how to characterize PAM-4 signals described in standards such as IEEE 802.3bs (200G/400G Ethernet) and the Optical Internetworking Forum-Common Electrical Interface–56G implementation agreement (CEI-56G-XX-PAM4), using the Keysight N109X DCA-M Series of Oscilloscopes.
Démonstration de base 2016-11-17 |
|
Using Source/Measure Unit as a Voltmeter - Demo Guide
This B2900A demo guide shows how easily you can use the B2900A series SMU as a voltmeter step by step via an example to measure voltage across a resistor.
Démonstration de base 2016-08-18 |
![]() |
Using Source/Measure Unit as an Ammeter - Demo Guide
This B2900A demo guide shows how easily you can use the B2900A series SMU as an ammeter step by step via an example to measure current from quasi current source circuit.
Démonstration de base 2016-08-17 |
![]() |
How to use AWG measurements to help with PAM-4 implementation
Learn how to use an arbitrary waveform generator and scopes to measure and analyze PAM-4 signals. Elements include transitioning from NRZ to PAM-4 signals, influencing the shape of the eye and the resulting spectral behavior, adding distortions to see receiver response, adding pre-distortion, and embedding your channel.
Démonstration de base 2016-02-29 |
|
Sequencing tests on B2900A SMUs using EasyEXPERT software
Watch a video of the EasyEXPERT group+ software introducing its sequencing test mode using the Keysight B2900A SMUs.
Démonstration de base 2016-02-17 |
|
Curve tracing on B2900A SMUs using EasyEXPERT software
Watch a video of the EasyEXPERT group+ software introducing its curve tracing mode using the Keysight B2900A SMUs.
Démonstration de base 2016-02-17 |
|
How to test PCIe 4.0
The spec for PCIe 4.0 (gen4) is not finalized, but testing is still required. See a demonstration of a test solution on an Analog Bits half power SERDES running at 16 Gb/s to help get your PCIe gen4 device running. Calibrated stressed output, ISI, and jitter tolerance tests ready for PCIe 4.0.
Démonstration de base 2016-02-12 |
|
1 2 3 4 5 Page suivante