您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-3 / 3

排序:
Is the collet (center contact) of the 16454A identical to that of the 42942A (part number 1250-0907)?
Yes, When replacing the collet (center contact) of the 16454A, you can use the same part (part number 1250-0907) as that used in the 42942A.

FAQ 2009-01-12

Can I replace the 16008B's conductive elastomer when it is deteriorated?
No, since the conductive elastomer cannot be removed from the main electrode assembly of the 16008B, replace whole main electrode assembly with new one.

FAQ 2008-05-16

How can I order supplemental parts for component test fixtures/accessories?
You can order the necessary parts by the part numbers shown in the Accessories Selection Guide for Impedance Measurements.

FAQ 2008-04-22