Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

Categoria de Produto

1-13 de 13

Sort:
What is the CPU / Storage / Windows OS history?
The history of CPU type/memory size, storage type/size, windows OS is listed in the table.

FAQ 2018-08-21

How does the Microsoft end of support for Windows XP affect my ENA?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will help you answer some important questions.

FAQ 2015-07-27

How does the Microsoft end of support for Windows XP affect my E4982A?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will help you answer some important questions.

FAQ 2014-04-24

Can I use a USB memory to update the firmware for the ENA?
It depends on the model.

FAQ 2012-12-28

Is it possible to disable or enable the Automatic Logon for Windows on the ENA?
Yes. To disable or enable the Automatic logon for Windows in a Non-Domain System, perform the following:

FAQ 2012-12-18

How can I check for the computer viruses on the ENA?
It depends on the model...

FAQ 2012-12-11

Can I install extra applications on the ENA?
It depends on the model...

FAQ 2012-12-11

The ENA / ENA-L was infected with the virus. What should I do?
Remove the LAN cable and perform system recovery.

FAQ 2011-10-07

Anti-Virus FAQ for ENA

FAQ 2011-10-07

Does the ENA-L support a built-in web page similar to the 871x family?

FAQ 2011-10-07

Does Sweep End signal output on 24-bit I/O port of the 4294A have similar definition as End of Measure (EOM) signal on LCR meters?
Sweep End signal means the end of entire sweep measurement, not the end of measurement at each sweep point.

FAQ 2010-07-02

Is it possible to parallel more than 2 units of the 42841A to expand bias current output range?
No. Instrument does not have firmware to control more than 2 units of the 42841A. In addition, connecting more than 2 units of the 42841A may cause an "OVLD" status due to possible imbalance of DC bias source and sink currents.

FAQ 2008-05-26

Can I use any instrument driver supporting the 4294A?
Yes. The LabView driver for the 4294A is available.

FAQ 2008-05-26