検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

コンテンツのタイプ

製品カテゴリ

1-25 / 34

並べ替え
Keysight E4980Aの"DC Source Option 001 (±10 VDC Max)"とは何ですか?どのように使用するのですか?
E4980Aのオプション001「電源およびDCバイアス機能拡張オプション」で提供される機能拡張の概要。

FAQ 2012-12-11

2台のKeysight 4287Aインピーダンス・アナライザ間でテスト・ヘッドを交換するとどうなりますか?
Keysight 4287Aインピーダンス・アナライザは、セットとして付属しているテスト・ヘッドを使用する必要があります。付属のテスト・ヘッドは4287Aの一部として校正され分離できないためです。

FAQ 2012-01-30

ENA-Lは871xシリーズのような内蔵Webページをサポートしていますか?
いいえ、していません。

FAQ 2011-10-07

ENAアナライザとSCPI-LANで通信するためHP Basicを設定する際の情報はありますか?
ENAのLAN設定を認識するためにHP Basic AUTOSTを設定します。

FAQ 2011-10-07

E4991AのVBAマクロ機能を使って外部GPIB機器を制御するのに必要なインタフェース・ケーブル/アダプタは?
E4991AのOSのバージョンによっては、10833A/B/C/D、82357Aまたは82357Bが必要です。

FAQ 2011-06-19

4294A用IntuiLinkソフトウェアが動作しているときに、PCに"Failed to Capture State from Instrument"と表示される理由は?
4294AのファームウェアがRev 1.11よりも前である場合は、以下のエラー・メッセージが表示されます。

FAQ 2011-06-19

Why isn't calibration option (UK6) available for the 42941A?
The 42941A does not have calibration option because the 4294A specifies total measurement accuracy including the 4294A accuracy.

FAQ 2010-07-12

Is it possible to separate the test head from the E4991A and interconnect them with cables?
Yes. It is possible with option E4991A-010 or option E4991A-007 only.

FAQ 2010-07-02

E4991Aオプション010が必要なのは、E4991Aで特定のプローブ・ステーションを使用する場合だけですか?
いいえ。E4991A-010は一般に、E4991Aとプローブ・ステーションを組み合わせて使用する場合に必要です。

FAQ 2010-05-12

E4991Aのテスト・ポートの拡張に使用できるオプションまたはアクセサリはありますか?
E4991A-007温度特性テスト・キット以外は、E4991Aのテスト・ポートを拡張するためのオプションもアクセサリも用意されていません。

FAQ 2010-04-29

16453Aまたは16454Aと組み合わせて使用しなくても、E4991Aオプション002で誘電率または透磁率を測定できますか?
できません。E4991Aオプション002を使用して誘電率または透磁率を測定する場合は、16453Aまたは16454Aが必要です。

FAQ 2010-04-29

41951Aインピーダンス・テスト・キットを4295A/4296Bと組み合わせて使用することはできますか?
できません。41951Aは4295Aまたは4296Bと組み合わせて使用することはできません。

FAQ 2010-04-25

Keysight Intuilink 4395Aを、4395A、4396Bアナライザと接続した時に生じる異常
4395A、4396Bコンビネーション・アナライザと組み合わせて使用するためにKeysight Intuilink Agt4395データ収集ユーティリティをインストールしました。

FAQ 2009-11-05

Is calibration report included in the 16380V-001 Upgrade Kit which adds the 10 µF standard capacitor to the 16380C?
Yes, the 16380V-001 Upgrade Kit includes the 10 µF standard capacitor and its calibration report.

FAQ 2009-06-23

How do I connect the 16048G 1m BNC connector leads to the 16452A?
You need four BNC(m) to BNC(m) adapters (Keysight part number 1250-0216) to connect the 16048G to the 16452A.

FAQ 2009-01-12

Does the E4980A have 2 m / 4 m cable length option?
No option is required because the standard model of the E4980A has the cable length correction function for 0 m, 1 m, 2 m and 4 m test leads.

FAQ 2008-11-12

Are there any restrictions on the selection of the E4980A options?
The E4980A-001 "Power and DC Bias Enhancement" and E4980A-002 "Bias Current Interface" can be installed in the same unit but cannot be operated simultaneously.

FAQ 2008-11-12

Can the E4980A with option E4980A-005 be upgraded to standard model?
Yes. The E4980A-005 can be upgraded to the standard model by ordering the E4980AU-007 Upgrade Kit. The upgrade can be performed at Keysight service center only.

FAQ 2008-11-12

Can I integrate the 4287A into a semiconductor probe station?
The 4287A can be integrated in a semiconductor probe station, but is not suitable for C-V and high impedance measurement applications for the following reasons:

FAQ 2008-06-11

Can I use the 16048A/D/E with the 4294A?
No, the 4294A adapter setup function only supports 16048G/H cables to extend calibration plane. The 16048A/D/E are not available for the adapter setup and cannot provide accurate and specified measurements.

FAQ 2008-05-26

Can I order brand-new 16380A with ANSI Z540 accredited calibration?
Yes, the 16380A with the ANSI Z540 calibration can be ordered. Order the 16380A with R1295A.

FAQ 2008-05-22

Can I order brand-new 16380C with ANSI Z540 accredited calibration?
Yes, the 16380C with the ANSI Z540 calibration can be ordered. Order the 16380C with R1295A.

FAQ 2008-05-22

Can I order each standard resistor of the 42030A independently?
No, each standard resistor of the 42030A cannot be ordered to purchase independently.

FAQ 2008-05-20

Can I use the 16454A with an LCR meter or Impedance Analyzer other than the E4991A-002 or 4291A/B-002?
Yes, basically, it is recommended to use an Impedance Analyzer with I-Basic programming function in order to automate the permeability calculation.

FAQ 2008-05-20

Is calibration report furnished to the 16380A?
Yes, the COC and the calibration report for all 4 standard capacitors are furnished. No option is required for the calibration report furnished.

FAQ 2008-05-20

1 2 次へ