您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 525

排序:
Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

Where can I find information on E4980A/AL error messages?
E4980A/AL error messages are described in Appendix B of the Users Guide.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

How do I upgrade my 4396B Network/Spectrum/Impedance Analyzer?
Information for hardware and software options upgrade

FAQ 2016-02-26

什麼是增強型超載檢測和電源跳閘功能?
自 2015 年秋季起,E5061B 選項 115/117/135/137/215/217/235/237 開始標配增強型超載檢測和電源跳閘功能。E5061B 選項 3L5 不具備這種功能。

FAQ 2016-01-28

我要如何將 E5061B ENA 系列網路分析儀升級?
硬體與軟體選項升級資訊

FAQ 2016-01-27

Microsoft 不再支援 Windows XP 對我的 ENA 有何影響?
Microsoft 於 2014 年 4 月 8 日停止對 Windows XP 作業系統的支援。請閱讀此頁面以了解我們對此問題的解答。

FAQ 2015-07-27

E4990A 硬體、軟體及韌體升級
E4990A 阻抗分析儀升級選項完整清單

FAQ 2015-07-03

How do I upgrade my E4991B Impedance Analyzer?
Information for hardware and software options upgrade

FAQ 2015-06-19

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

我要如何使用 ENA 進行 75 Ω 量測?
您可以將系統特性阻抗改成 75 Ω,使用 ENA 進行 75 Ω 量測。

FAQ 2015-03-09

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

E4982A 硬體、軟體及韌體升級
E4982A 硬體、軟體及韌體升級

FAQ 2014-05-01

CPU / 儲存類型 / Windows OS 歷史紀錄
表格中列出過去的CPU類型/記憶體容量、儲存類型/容量、windows OS。

FAQ 2014-04-28

Microsoft 不再支援 Windows XP 對我的 E4982A 有何影響?
Microsoft 於 2014 年 4 月 8 日停止對 Windows XP 作業系統的支援。請閱讀此頁面以了解我們對此問題的解答。

FAQ 2014-04-24

What are the differences between the E4980A and 4284A?
Most of the E4980A functions are compatible with the 4284A's. Since some enhancements and updates of functionality are incorporated in the E4980A, there are primary differences summarized in the table.

FAQ 2014-04-07

從只配備GP-IB介面的各種是德分析儀來列印及擷取螢幕影像的替代方案有哪些?

FAQ 2014-02-08

E4980A 和 42841A 之間的纜線的產品編號是什麼?
目前的纜線的產品編號是 E4980-61640。

FAQ 2014-02-06

Replacing the 8508A vector voltmeter with the E5061B network analyzer
Measuring the phase difference of an external CW signals is a typical measurement application of the 8508A vector voltmeter.

FAQ 2013-10-14

How can I order the upgrade kit of the 4395A
The model numbers of available upgrade kits for the 4395A options are as follows.

FAQ 2013-06-24

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

我在哪裡可以找到過時的HP測試儀器的使用手冊?
有一些公司可能還會提供這些使用手冊…

FAQ 2013-05-29

1 2 3 4 5 6 7 8 9 10 ... 下一頁