Техническая поддержка
Электронные измерения
Уточнить список
По теме
- Calibration (43)
- Configuration & Installation (34)
- Display Messages/Error Codes (25)
- Measurement & Instrument Fundamentals (52)
- Measurement Techniques (102)
- Operating System & Software (13)
- Operation & Functionality (231)
- Other Information (17)
- Parts & Accessories (110)
- Printing & Printers (6)
- Product & Firmware Updates & Upgrades (36)
- Product Theory of Operation (7)
- Programming & Data Transfer (74)
- Service & Maintenance (20)
- Specifications & Accuracy (44)
- Troubleshooting (9)
По типу содержания
- FAQ (526)
По типу оборудования
-
Все типы оборудования
-
Осциллографы, анализаторы, измерители
- Измерители LCR и приборы для измерения импеданса
-
Осциллографы, анализаторы, измерители
201-225 из 526
How to calculate the accuracy for U1731B/U1732B Inductance Measurements?
The accuracy is calculated using the formula in the data sheet...... The Example......
FAQ 2010-05-05 |
|
Does the 4294A have the ALC (Auto Level Control) function?
No, the 4294A doesn't have the ALC. I-Basic program can be used to achieve the test signal ALC.
FAQ 2010-05-03 |
|
How to calculate the accuracy for U1731B/U1732B Capacitance Measurements?
The accuracy is calculated using the formula in the data sheet...... The Example......
FAQ 2010-05-03 |
|
Can the E4991A option 002 measure permittivity or permeability without being used with the 16453A or 16454A?
No. The 16453A or 16454A is required when the E4991A option 002 is used to measure permittivity or permeability.
FAQ 2010-04-29 |
|
Is there any option or accessory available for extending the test port of the E4991A?
Except for the E4991A-007 temperature characteristic test kit, neither option nor accessory for extending the test port of the E4991A has been set up.
FAQ 2010-04-29 |
|
How should I perform Load compensation when using the 16451B with the 4294A?
Utilize an air-dielectric capacitance of the 16451B's parallel plate electrodes as the load device and perform the load compensation.
FAQ 2010-04-29 |
|
Why is a black paint adhered on one side of the air-line center conductor of the 16190B?
The black paint is a marking to indicate the directivity of the center conductor connected to the test port.
FAQ 2010-04-29 |
|
Can the DC bias monitor (Vdc and Idc) function of the E4980A and 4294A be used to measure a DC voltage or current other than internal DC bias?
No. The Vdc and Idc monitor function can only be used to verify internal DC bias voltage and current.
FAQ 2010-04-13 |
|
Can the 41951A Impedance Test Kit be used with the 4395A/ 4396B?
No, the 41951A cannot be used with the 4395A or 4396B.
FAQ 2010-04-13 |
|
Is there any simple method of having the E4980A start up with a low test signal voltage?
You can have the E4980A start up with a low test voltage by saving a test level setting in memory and starting up with the recalled setting.
FAQ 2010-03-31 |
|
How do I order replacement pin tips for my Keysight 42941A Impedance Probe?
Order Keysight part number 42941-60004.
FAQ 2010-03-16 |
|
Can the U1731B/U1732B Handheld LCR Meter measure a battery's internal resistance?
No, the U1731B and U1732B Handheld LCR meters cannot measure active parts like batteries etc.....
FAQ 2010-02-21 |
|
Are there any programming commands for the U1701B Handheld Capacitance Meter?
No, it only offers datalogging with Keysight U1701B GUI Data Logger Software…
FAQ 2010-02-21 |
|
Are there any programming commands for the U1731B/U1732B Handheld Capacitance and LCR Meter?
No, it only offers datalogging with Keysight U173xB GUI Data Logger Software.
FAQ 2010-02-21 |
|
How can I check for anomaly in test fixture when the E4980A/ 4263B/ 4284A/ E4981A fails in open/short compensation for a particular test fixture?
FAQ 2010-01-26 |
|
Does the 4396B immediately shut off the RF signal source when the RF OUT On/Off key is pushed?
It depends on the 4396B firmware revision.
FAQ 2010-01-26 |
|
Can the E4980A/ 4284A measure DUT when "Warning, ALC unable to regulate" is displayed?
Yes, the E4980A/ 4284A can measure DUT though the test signal level is not controlled at the ALC setting value.
FAQ 2010-01-26 |
|
When the 4287A displays inaccurate Rdc measurement values, what is required to make more proper Rdc measurements for contact check?
Perform Open/Short/Load calibration and Open/Short compensation.
FAQ 2010-01-26 |
|
Why does the DC current bias system indicate incorrect measurement values when the 42841A is turned off?
FAQ 2010-01-26 |
|
What is the recommended calibration period of the 16190B?
The recommended calibration period is every 12 months.
FAQ 2009-11-17 |
|
What is the recommended calibration period of the 42030A?
The recommended calibration period is every 12 months.
FAQ 2009-11-17 |
|
What is the recommended calibration period of the 16380C?
The recommended calibration period is every 12 months.
FAQ 2009-11-17 |
|
What is the recommended calibration period of the 16380A?
The recommended calibration period is every 12 months.
FAQ 2009-11-17 |
|
Anomalies connecting Keysight Intuilink 4395A to the 4395A, 4396B Analyzers
FAQ 2009-11-02 |
|
Are there any programming commands for the U1731A/U1732A Handheld Capacitance and LCR Meter?
No, it only offers datalogging with Keysight U173xA GUI Data Logger Software.
FAQ 2009-10-26 |
|