Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 31

Упорядочить:
Signal Analyzer LabVIEW Instrument Drivers
Supported models: N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, N8973B, N8974B, N8975B, N8976B, M8920A

FAQ 2017-12-01

What comes standard or pre-configured in my NFA X-Series analyzer and what options are available at the time of initial purchase?
See the list by selecting the link...

FAQ 2016-04-08

What measurement applications can I install on my NFA X-Series Noise Figure Analyzer?
Short list can be found here...

FAQ 2016-03-03

Обновление измерительных приложений и прошивки для анализаторов сигналов
Самые последние версии измерительных приложений и прошивки для анализаторов сигналов

FAQ 2015-03-04

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

Is there a sample program for acquiring Noise Figure and Gain Data from the NFA Series of Noise Figure Analyzers?
Yes

FAQ 2014-01-31

Is it possible to improve the system noise figure and reduce the measurement uncertainty of the Keysight N897xA Series Noise Figure Analyzers when c...

FAQ 2014-01-31

How does the attenuation algorithm in the NFA work?
See this FAQ for details

FAQ 2014-01-31

On the Keysight NFA Series of Noise Figure Analyzers, is it possible to query the RF attenuator range while in the auto range mode?
The command to query the Keysight NFA RF attenuator while in the auto ranging mode is: DIAG:BLU:RF:RANG?

FAQ 2014-01-31

What is the absolute output power level of the various Keysight noise sources?

FAQ 2012-11-06

What is the Noise Figure accuracy specification for measuring “my device”?
Keysight supplies a web-based noise figure measurement uncertainty calculator. More details about how to use this tool can be found here...

FAQ 2012-07-31

For Cable Testing should I use a TDR, a network analyzer, or both?
The cable specifications will determine the test equipment requirements...

FAQ 2011-10-07

Is there an example program for acquiring data from the Keysight 8970B Noise Figure meter via the GPIB bus?
Vee program found here...

FAQ 2009-04-28

Is it possible to reset the 8970A,B Noise Figure instrument storage/recall states to factory defaults?
Key sequence can be found here...

FAQ 2009-04-28

Can the 346C-K01 be used below 1 GHz?
This special option is not calibrated or characterized below 1 GHz.

FAQ 2009-04-28

Is it possible to plot Noise Figure and Gain traces from the 8970B to a printer via the Intelligent Interfaces Converter?
Yes, as long as the converter can still be purchased.

FAQ 2009-04-28

What are the differences between the 8970A and 8970B Noise Figure Meters?
Details can be found here...

FAQ 2009-04-28

Is it possible to reset the 8970A,B Noise Figure ENR table values to factory default?
Button sequence found here...

FAQ 2009-04-28

During a mixer noise figure test (NF) why are the NF and gain not equivalent to zero after a user calibration?
Details can be found here...

FAQ 2009-04-28

Which of Keysight's sensor cables and power meters are compatible with each other?
The table given here shows the compatibility between Keysight's sensor cables and power meters:….

FAQ 2009-02-27

What does Error Code 27 on the 8970B Noise Figure Analyzer indicate?
The Keysight 8970B/71B/71C Noise Figure Measurement Operating Manual specifies the error code as: “Overflow while calibrating”.

FAQ 2009-02-09

What does Error Code 18 on the 8970B Noise Figure Analyzer Indicate?
Frequency calibration failed.

FAQ 2009-02-09

What do the various error codes on the 8970B Noise Figure Meter indicate?
Refer to the 8970B Error Message Data Sheet

FAQ 2009-02-09

What does Error Code 22 on the 8970B Noise Figure Analyzer indicate?
Current RF attenuation not calibrated.

FAQ 2009-02-09

What is the minimum sensitivity of the N897xA NFA Series?
Sensitivity is not a specified parameter

FAQ 2009-02-09

1 2 Следующие