您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-6 / 6

排序:
How do I measure accurately below -60dBm using U2040 X-Series Sensor?
Click on the question above for recommended steps.

FAQ 2015-12-14

What is the correct linearity setting for V8486A & W8486A sensor?
The automatic selection must be overridden: select the D type linearity for this sensor.

FAQ 2010-05-10

How does the measurement accuracy of the N8480 series Power Sensors compare to that of the legacy 8480 series sensors?
The N848xA Power Sensors are as accurate if not more accurate than the legacy 848xA sensors they replace….

FAQ 2009-12-15

What is option H12 for the E4418B and E4419B EPM Series Power Meters?
Option H12 for the E4418B and E4419B EPM Series Power Meters provides an improved power level accuracy specification....

FAQ 2009-04-12

我能在 478A 同軸熱敏電阻安裝感測器上換裝選項 H75 或 H76 嗎?
因不能在現有的 478A 上換裝選項 H75 和 H76。在最初購買 478A 的同時便必須訂購任其中一個選項。

FAQ 2005-05-19

我如何設定 E932XA 系列功率感測器的 EPM-P E4416A 或 E4417A 功率錶,以便在如 -50 dBm 的低功率位準時獲得最準確的量測?
若看到可疑的結果,最有可能是選取不正確的操作模式。E932XA 系列感測器「正常模式」的動態範圍是 65-70dB,而「僅平均模式」的則為 80-85dB (視感測器機型而定)。

FAQ 2005-04-20