您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 51

排序:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-04

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

我在哪裡可以找到過時的HP測試儀器的使用手冊?
有一些公司可能還會提供這些使用手冊…

FAQ 2013-05-29

What is the latest version of protocol software for my protocol analyzer (PCI Express, HDMI, or Fibre Channel)?
See the list of current software versions available.

FAQ 2012-08-24

What application software is available for 16900, 1680x, 1682x and 1680/1690 Series logic analyzers?
See the table for quickly seeing the application support available for Keysight U4000, 16900, 16800 and 1680/90 logic and protocol analyzers.

FAQ 2012-08-14

I have loaded an LDF, and pressed "Start", but do not see any traffic in the trace. How can I fix this?
Make sure all nodes in your network are activated for emulation. Go to the Windows menu, and select "Nodes/Frames/Signals". For all nodes that you want to emulate, select the node, and after right-clicking on it, select "Emulate Node".

FAQ 2010-07-23

How can I check for a proper serial connection?
Make sure the serial cable is securely connected to the COM port on your PC, and to the connector marked "PC RS232" on the LIN Tester…

FAQ 2010-07-23

Where can I find documentation for the PCIe Analyzer/Exerciser?
The best documentation is found in the online help installed on the controller.

FAQ 2009-08-25

Does the Keysight E2960B, also known as N5309A, Exerciser have a signal or chip reset for the output signal?
Yes. There is a TCL command for this.

FAQ 2009-08-10

What is the actual size of the E2960B (N5309A) PCIe Exerciser Data Memory?
The E2960B (N5309A) PCI Express internal data memory is 256K.

FAQ 2009-08-10

How can I find out the serial number of the VPT501?
Start the Configuration Tool. Click “Scan”. All VPT501 Hardware Devices found are listed...

FAQ 2008-01-29

Why do I get a message that a help file or DLL was not found?
This message usually only occurs if you have chosen the “compact installation” setup type or “custom installation”...

FAQ 2008-01-29

Why are the networks disconnected on certain actions regarding the MCF file?
To avoid inconsistent software behavior, the networks are disconnected automatically before the MCF is reloaded or a reference MCF is saved...

FAQ 2008-01-29

Is there a sample project that demonstrates the operation of the VPT501?
Yes, there are 2 sample projects to be found in the directory “Samples” in the program installation directory...

FAQ 2008-01-29

When loading an LDF, LIN Tester reports Error ( 773,20 ): More than 16 Schedule Tables. Why?
Due to memory resources in the LIN Spector, the allowed number of schedule tables is limited to 16.

FAQ 2007-10-05

When loading LDF, LIN Tester reports Error message (826,30): More than 64 Entries in Schedule Table:Config. Why?
Due to the limited memory in the LIN Spector the number of allowed entries in a schedule table is limited to 64.

FAQ 2007-10-05

How can I find out the serial number of my LIN Tester?
Go to Help->About. The screen will show the serial number and all software versions of the installed modules.

FAQ 2007-09-21

Can I connect a LINspector from Volcano/Mentor to the Keysight software?
Only hardware shipped from Keysight is supported by the Keysight Software (and vice versa). You need to upgrade your hardware to a Keysight J8115A.

FAQ 2007-09-21

How do I know whether the LIN Tester is properly powered?
Check the red LED next to the Network connector. It will be lit when power is available.

FAQ 2007-09-21

為什麼我無法在Windows 2000/XP 中安裝 Keysight E2929B USB 驅動程式?

FAQ 2005-07-07

我要如何自中斷的韌體升級還原 Keysight E2929B?

FAQ 2005-07-05

使用 Keysight E2928A 時,我要如何在目標中止之後停止主要的複試?
這是Keysight E2928A 主要狀態機的限制。解決無法重新開機的方法即是利用 BestSMReset 命令透過 API 停止主機

FAQ 2005-06-30

為什麼 PCI2.1 裝置無法在 SVP3.0 上使用,PCI2.3 裝置無法在 SVP1.7 上使用?
PCI 2.3 版的 PCI 技術規格命令暫存器中已經過修改。由於 SVP3.0 中測試 PCI2.3 規格,而 SVP1.7 中測試 PCI2.1 規格,因此 2.1 的相容裝置無法使用 SVP3.0,PCI2.3 相容裝置中無法使用 SVP1.7。

FAQ 2005-06-23

E2930B 可和 PCI 或 PCI-X 1.0 共用嗎?
E2930B 完全支援 PCI-X 1.0 和 PCI-X 2.0 技術規格。它可完全取代 E2929B。對於傳統的 PCI,E2930B 提供了設定的空間,讓您以 33 MHz 讀取和寫入資料。

FAQ 2005-06-23

為什麼我在使用新版 E2920A 軟體執行 PPR 時,收到的分批回應比以前還多?
為什麼我在使用新版 E2920A 軟體執行 PPR 時,收到的分批回應比以前還多?

FAQ 2005-06-23

1 2 3 下一頁