您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 465

排序:
Example Program for Reading Binary Data (Python 3)
Reads binary data saved by the Keysight InfiniiVision Series oscilloscopes.

程式編寫範例 2019-12-16

ZIP ZIP 3 KB
MATLAB sample program
MATLAB sample program on how to convert the data return by TRACe:DATA? to a plot to show the trace in MATLAB.

程式編寫範例 2018-07-25

ZIP ZIP 1 KB
E4980A/AL Data Transfer Program (Excel VBA)
This program (a VBA macro for Microsoft Excel) transfers the list sweep measurement data from the E4980A to a PC.

程式編寫範例 2018-06-14

System-Level Rise and Fall Time Verification Utility
A utility to verify system-level rise and fall Time performance of the N1921/2A wideband power sensor.

程式編寫範例 2018-03-06

ZIP ZIP 97 KB
E4990A material measurement software - trial version
This program assists material measurements (permittivity or permeability) using the E4990A Impedance Analyzer with the 16451B Dielectric Test Fixture, the 16452A Liquid Test Fixture, and the 16454A Magnetic Material Test Fixture. This program is a VBA macro for Microsoft Excel, performs instrument setup and calibration, data transfer, parameter conversion, and data plot. Note: the expiration date of this trial version software is April. 10, 2018.

程式編寫範例 2018-01-29

ZIP ZIP 5.68 MB
A Program to retrieve Cal Factor for Power sensor.
A Program to retrieve Cal Factor for Power sensor.

程式編寫範例 2017-11-29

ZIP ZIP 43 KB
Get Screen Image, VISA library, Python (2.7)
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

程式編寫範例 2017-04-28

ZIP ZIP 3.27 KB
Get Screen Image, VISA library, Python 3.5
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

程式編寫範例 2017-04-28

ZIP ZIP 2.32 KB
Get *IDN? Query Results, VISA COM library, C#
This sample program sends a *IDN? SCPI query to an instrument to get its identification string. The result is displayed on a MS Windows Console.

程式編寫範例 2017-04-28

ZIP ZIP 41.79 KB
Get Segmented Memory Time Tags and Measurement Results, VISA COM library, VBA
This sample program assumes the oscilloscope has been set to capture N segments. The program lists the segment number and the relative time stamp of that segment. A Delay measurement is made between channels 1 and 2 within each segment and the measurement value from each segment is listed.

程式編寫範例 2017-04-28

ZIP ZIP 33.08 KB
Acquisition Synchronization, Two Simple Methods, MATLAB
This script shows how to properly initialize a Keysight InfiniiVision or InfiniiVision X-Series oscilloscope and synchronize an acquisition using the blocking :DIGitize command.

程式編寫範例 2017-04-28

ZIP ZIP 328.53 KB
Get Screen Image and Waveform Data and Save to USB Thumb Drive, VISA library, Python
This script shows how to save a screen image and waveform data to a USB stick, with error checking.

程式編寫範例 2017-04-28

ZIP ZIP 5.50 KB
Get *IDN? Query, Screen Image, and Waveform Data Results, VISA COM library, VBA
This sample program performs three different tasks: 1) sends a *IDN? query to the instrument and reads back the ID string, 2) captures and saves a screen image from the oscilloscope, and 3) gets the oscilloscope's waveform data from channels 1 and 2.

程式編寫範例 2017-04-28

ZIP ZIP 1.30 MB
Get Waveform Data (Elegant), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

程式編寫範例 2017-04-28

ZIP ZIP 13.93 KB
Load Arbitrary Waveform Data into WaveGen, VISA library, Python
This example shows several methods for getting arbitrary waveform data into the waveform generator of a Keysight InfiniiVision X-Series oscilloscope. The oscilloscope must have the WaveGen license and support arbitrary waveforms.

程式編寫範例 2017-04-28

ZIP ZIP 6.08 KB
Get Lister Data, VISA library, Python 3.5
This script is a reference and starting point for automating Lister data capture over USB.

程式編寫範例 2017-04-28

ZIP ZIP 4.21 KB
Get Segmented Memory Time Tags and Measurement Results, VISA library, Python
This script figures out how many segments were acquired, flips through them, gathers the time tags and desired measurement results.

程式編寫範例 2017-04-28

ZIP ZIP 4.96 KB
Get Waveform Data (Brute Force), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

程式編寫範例 2017-04-28

ZIP ZIP 13.62 KB
Get Waveform Data, VISA COM library, VBA
This sample program gets waveform data from the oscilloscope.

程式編寫範例 2017-04-28

ZIP ZIP 1.01 MB
Get InfiniiVision X-Series Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion X-Series oscilloscope.

程式編寫範例 2017-04-28

ZIP ZIP 65.53 KB
Acquisition Synchronization, Two Simple Methods, VISA library, Python
This script shows the two best synchronization methods for all InfiniiVision and InfiniiVision X-Series oscilloscopes. Benefits and drawbacks of each method are described.

程式編寫範例 2017-04-28

ZIP ZIP 338.73 KB
Get Segmented Memory Time Tags, Waveforms, and Measurement Results, VISA library, Python
This script can get waveforms and measurements from analog channels for segmented memory already acquired on an InfiniiVision oscillocope. It can also get time tags and produce an averaged segment for each analog channel.

程式編寫範例 2017-04-28

ZIP ZIP 8.17 KB
Get Waveform Data, VEE
This sample program gets waveform data from the oscilloscope.

程式編寫範例 2017-04-28

ZIP ZIP 4.08 KB
Get InfiniiVision Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion oscilloscope.

程式編寫範例 2017-04-28

ZIP ZIP 48.93 KB
Get Waveform Data, LabVIEW
This sample program gets waveform data from the oscilloscope.

程式編寫範例 2017-04-28

ZIP ZIP 69.15 KB

1 2 3 4 5 6 7 8 9 10 ... 下一頁