Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 466

Sort:
Example Program for Reading Binary Data (Python 3)
Reads binary data saved by the Keysight InfiniiVision Series oscilloscopes.

Programming Example 2019-12-16

ZIP ZIP 3 KB
A Program to retrieve Cal Factor for Power sensor - EXE .
A Program to retrieve Cal Factor for Power sensor - EXE .

Programming Example 2019-12-12

EXE EXE 94 KB
[Method of Implementation] Ethernet Cable-Interconnect Compliance Test Solutions

Programming Example 2019-10-02

MATLAB sample program
MATLAB sample program on how to convert the data return by TRACe:DATA? to a plot to show the trace in MATLAB.

Programming Example 2018-07-25

ZIP ZIP 1 KB
[VBA Sample Program] Resistivity Measurement of Insulating Materials for B2985A/87A
VBA sample program for B2985A/87A electrometers/high resistance meters to measure volume and surface resistivity of insulating materials by using the N1424A/B/C Resistivity Cell. Operation guide and requirements are included in the Microsoft® Excel file.

Programming Example 2018-06-29

E4980A/AL Data Transfer Program (Excel VBA)
This program (a VBA macro for Microsoft Excel) transfers the list sweep measurement data from the E4980A to a PC.

Programming Example 2018-06-14

System-Level Rise and Fall Time Verification Utility
A utility to verify system-level rise and fall Time performance of the N1921/2A wideband power sensor.

Programming Example 2018-03-06

ZIP ZIP 97 KB
E4990A material measurement software - trial version
This program assists material measurements (permittivity or permeability) using the E4990A Impedance Analyzer with the 16451B Dielectric Test Fixture, the 16452A Liquid Test Fixture, and the 16454A Magnetic Material Test Fixture. This program is a VBA macro for Microsoft Excel, performs instrument setup and calibration, data transfer, parameter conversion, and data plot. Note: the expiration date of this trial version software is April. 10, 2018.

Programming Example 2018-01-29

ZIP ZIP 5.68 MB
A Program to retrieve Cal Factor for Power sensor-- Vee Runtime (VXE) .
A Program to retrieve Cal Factor for Power sensor-- Vee Runtime (VXE) .

Programming Example 2017-11-29

ZIP ZIP 43 KB
Get Waveform Data (Brute Force), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

Programming Example 2017-04-28

ZIP ZIP 13.62 KB
Get Segmented Memory Time Tags and Measurement Results, VISA library, Python
This script figures out how many segments were acquired, flips through them, gathers the time tags and desired measurement results.

Programming Example 2017-04-28

ZIP ZIP 4.96 KB
Get Waveform Data (Elegant), VISA library, Python
This script shows how to pull the waveform data from the analog channels for already acquired data and save it to a computer. It shows how to determine which channels are on and have data, how much data, get the data into an array, scale data for each channel, and save/recall it to/from disk in both csv and Python Numpy formats.

Programming Example 2017-04-28

ZIP ZIP 13.93 KB
Get Screen Image, VISA library, Python (2.7)
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

Programming Example 2017-04-28

ZIP ZIP 3.27 KB
Get *IDN? Query Results, VISA COM library, C#
This sample program sends a *IDN? SCPI query to an instrument to get its identification string. The result is displayed on a MS Windows Console.

Programming Example 2017-04-28

ZIP ZIP 41.79 KB
Get Waveform Data, VEE
This sample program gets waveform data from the oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 4.08 KB
Acquisition Synchronization, Two Simple Methods, VISA library, Python
This script shows the two best synchronization methods for all InfiniiVision and InfiniiVision X-Series oscilloscopes. Benefits and drawbacks of each method are described.

Programming Example 2017-04-28

ZIP ZIP 338.73 KB
Get Segmented Memory Time Tags and Measurement Results, VISA COM library, VBA
This sample program assumes the oscilloscope has been set to capture N segments. The program lists the segment number and the relative time stamp of that segment. A Delay measurement is made between channels 1 and 2 within each segment and the measurement value from each segment is listed.

Programming Example 2017-04-28

ZIP ZIP 33.08 KB
Get Segmented Memory Time Tags, Waveforms, and Measurement Results, VISA library, Python
This script can get waveforms and measurements from analog channels for segmented memory already acquired on an InfiniiVision oscillocope. It can also get time tags and produce an averaged segment for each analog channel.

Programming Example 2017-04-28

ZIP ZIP 8.17 KB
Get Lister Data, VISA library, Python 3.5
This script is a reference and starting point for automating Lister data capture over USB.

Programming Example 2017-04-28

ZIP ZIP 4.21 KB
Get Waveform Data, LabVIEW
This sample program gets waveform data from the oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 69.15 KB
Acquisition Synchronization, Two Simple Methods, MATLAB
This script shows how to properly initialize a Keysight InfiniiVision or InfiniiVision X-Series oscilloscope and synchronize an acquisition using the blocking :DIGitize command.

Programming Example 2017-04-28

ZIP ZIP 328.53 KB
Get Screen Image and Waveform Data and Save to USB Thumb Drive, VISA library, Python
This script shows how to save a screen image and waveform data to a USB stick, with error checking.

Programming Example 2017-04-28

ZIP ZIP 5.50 KB
Get InfiniiVision X-Series Oscilloscope Screen Image, LabVIEW
This sample program captures and saves a screen image from the InfiniiVilsion X-Series oscilloscope.

Programming Example 2017-04-28

ZIP ZIP 65.53 KB
Get Screen Image, VISA library, Python 3.5
This script shows how to save a screen image from an InfiniiVision oscilloscope to a PC.

Programming Example 2017-04-28

ZIP ZIP 2.32 KB
Save and Recall Setups, VISA library, Python
This script shows how to query the oscilloscope setup, save it to disk, recall it form disk, and use it to set up the oscilloscope again. This is also shown using the *LRN? query and with just trigger setups.

Programming Example 2017-04-28

ZIP ZIP 4.39 KB

1 2 3 4 5 6 7 8 9 10 ... Next