您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依主題

依內容類型

依產品分類

1-25 / 49

排序:
Replacement of Control XTP, Module Control Card
Frequently Asked Questions about XTPA Module Control Card

FAQ 2013-06-11

Sample “testplan” for Utility card & FR3070A
Sample “testplan” for Utility card & FR3070A from manufacturing site

FAQ 2013-02-18

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

XVision fails to install on some laptops
Before installing XVision /ICT software, please follow the steps below:

FAQ 2012-09-25

使用 NFS share 時應如何設定檔案安全性與機板目錄?
一旦啟用「Client for NFS」,即可在網路上掛載任何網路檔案系統分享 (NFS share)。 有多種方式可設定 NFS share 的檔案安全性。

FAQ 2012-02-05

How can I access my i3070/3070 ICT board directories residing on Linux/UNIX controller, if I am running my ICT controller on Windows® 7?
Services for Network File System (NFS) and Subsystem for UNIX-based Applications (SUA) are the software packages provided by Microsoft® to enable the UNIX subsystem and other parts of the UNIX environment to be integrated onto the Windows environment.

FAQ 2011-11-01

What are the known conflicts between MKS NutCracker and Interix and the recommended workaround solutions?
There are three known key issues which you need to look out for:

FAQ 2011-11-01

How can I turn on the Services for NFS on Windows® 7 ICT controller?
Both the Windows 7 Ultimate and Windows Enterprise Edition contain the client for the Network File System (NFS) and Subsystem for UNIX-based Applications (SUA).

FAQ 2011-11-01

How can I turn on the SUA and its UNIX utility package on Windows® 7 ICT controller?
It is recommended that you DO NOT enable or install SUA. This is an optional feature and utility that is not needed for mapping NFS share.

FAQ 2011-11-01

How to access board directories resided on the Linux/Unix server using SAMBA/Common Internet File System (CIFS), if ICT controller is on Windows® 7?
SAMBA is a utility which allows you to share your files between Linux/UNIX and Windows®. By mounting the SAMBA share on your Linux/UNIX server, you can access the board files across the operating systems.

FAQ 2011-11-01

Eight commonly asked questions about the Medalist i3070 Series 5
The i3070 Series 5 sports various innovative hardware and software features to bring you much wider test coverage and superb throughput for cost savings and faster time to profit. Check out these key features.

FAQ 2011-08-08

What is an example of a routine in the testplan for flash programming using the Utility Card?
an example of a routine in the testplan for flash programming using the Utility Card

FAQ 2011-01-04

Are rules execution sequences arrange able? If yes, how to do it?
Expand the Device Navigation tree, select one of the rule, click "Up" or "Down" key to move the rule. See example below.

FAQ 2010-09-08

Keysight i3070 系統保固或支援合約是否涵蓋引導探棒?為什麼沒有?何時會生效?
否,引導探棒是 Keysight i3070 系統的配件,因此並不包含於系統保固和支援合約的範圍內。

FAQ 2010-05-04

What is the short-cut key to press to "login" to Engineer Test?
F9.

FAQ 2007-09-12

How to remove the "Component Navigation"?
Uncheck "View-Engineer-Component Navigation".

FAQ 2007-09-12

How to remove the "Test Execution"?
Uncheck "View-Engineer-Test Execution".

FAQ 2007-09-12

How to display short format for the Column Name?
Click "Edit-Preferences", go to Engineer Test Tab, select "Short" and click OK.

FAQ 2007-09-12

How to remove "Test Output"?
Uncheck all the above components in "View-Engineer-Test Output".

FAQ 2007-09-12

How do you add all the ICT user accounts and groups?
Double click the batch file at "Keysight_ICT\home\system\3070accounts.bat".

FAQ 2007-09-12

Can I run Auto-Optimizer with Control XT Card?
No, you must have Control XTP Cards to run Auto-Optimizer.

FAQ 2007-09-12

What should I ensure before execute "switch"?
Ensure that the licenses are in "Keysight_ICT\lib\i3070Mux" and in "Keysight_ICT\lib\i3070UnMux".

FAQ 2007-09-12

How do you install i3070 v7.00 software?
Please follow the instructions in "Installing or Upgrading to Medalist i3070 Software" (E9901-96001).

FAQ 2007-09-12

1 2 下一頁