Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

retirer tout le raffinement

Par sujet

By Type of Content

Par catégorie de produit

26-49 of 49

Sort:
Where is the "switch" application located?
C:\Agilent_ICT\util\switch.

FAQ 2007-09-12

Can user define the CPK for optimizer?
Yes. This menu can be accessed at "Actions-Optimizer-Rule Editor".

FAQ 2007-09-12

How to clear Output windows?
Click "View?Engineer?Clear Output" or Use short-cut key "Ctrl+Alt+A".

FAQ 2007-09-12

How to sort the Rule Name according to device types at Rule Database?
Select a device type in Ruleset navigation. Rule Database will show all the rule names that device type selected.

FAQ 2007-09-12

What is Auto-Optimizer?
Auto Optimizer is used to improve throughput.

FAQ 2007-09-12

What is the default directory that i3070 v7.00 installed?
C:\Agilent_ICT.

FAQ 2007-09-12

How to remove "Test Output"?
Uncheck all the above components in "View-Engineer-Test Output".

FAQ 2007-09-12

Where the licenses are stored initially?
"Agilent_ICT\lib\i3070Mux" or "Agilent_ICT\lib\i3070UnMux".

FAQ 2007-09-12

What is the short-cut key to press to do "testhead power on"?
Ctrl-Shift+P.

FAQ 2007-09-12

Can I run Auto-Optimizer with Control XT Card?
No, you must have Control XTP Cards to run Auto-Optimizer.

FAQ 2007-09-12

How do you access the Auto Debug rule editor?
"Actions-Auto Debug-Rule Editor".

FAQ 2007-09-12

How do you install i3070 v7.00 software?
Please follow the instructions in "Installing or Upgrading to Medalist i3070 Software" (E9901-96001).

FAQ 2007-09-12

How to remove the "Test Execution"?
Uncheck "View-Engineer-Test Execution".

FAQ 2007-09-12

How do you add all the ICT user accounts and groups?
Double click the batch file at "Agilent_ICT\home\system\3070accounts.bat".

FAQ 2007-09-12

What is the short-cut key for "faoff" at Engineer?
Shift+F2.

FAQ 2007-09-12

How does Auto-Guarding select a node for Guarding?
Each Guard node is "weighted" and the priority of which Guard node to use depends on the "weight" given to that node.

FAQ 2007-09-12

How to remove the "Component Navigation"?
Uncheck "View-Engineer-Component Navigation".

FAQ 2007-09-12

Can I run my test program from Agilent3070 directory?
Yes

FAQ 2007-09-12

What is the usage of the "on failure report"?
Allow the user to enter report failures such as 'parallel device' to the particular test.

FAQ 2007-09-12

What is "RunAllAIC"?
All unpowered analog tests will be executed based on AIC list. "Fail" result will be displayed only as "RED" color.

FAQ 2007-09-12

Why the commands that I type not supported in command line?
User can "filter off" to enable back filtered commands. But software may fail due to some commands are not supported.

FAQ 2007-09-12

Why my data didn't get save after edited Lower Tolerance Limit?
After manual edited parameters or options, 'Save Test' combo box must be checked before save.

FAQ 2007-09-12

How to display short format for the Column Name?
Click "Edit-Preferences", go to Engineer Test Tab, select "Short" and click OK.

FAQ 2007-09-12

How to stop and empty the test execution queue?
Click "Pause" button. Select all the tests in the queue by keying "Ctrl+a", click "Remove" button.

FAQ 2007-09-12

Previous 1 2