这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 153

排序:
Replacement of Control XTP, Module Control Card
Frequently Asked Questions about XTPA Module Control Card

FAQ 2013-06-11

What does the “peak” mode“, "base mode” and "integration time" mean on Keysight LED test?
The sensor will start sampling “LED” color and intensity when it receives a “trigger” command from the testplan. It will continue to samplethe “LEDs” color and intensity until a “learn” or “measure” command.

FAQ 2013-04-15

How do we test LEDs in a circuit that sets them to blink(turn on and off) at periods exceeding 400ms, eg 500ms on, 500 ms off?
The longest integration time for Keysight LED sensor is 400ms between the ‘trigger’ and ‘learn/measre’ commands.

FAQ 2013-04-15

Sample “testplan” for Utility card & FR3070A
Sample “testplan” for Utility card & FR3070A from manufacturing site

FAQ 2013-02-18

What are the failures that boundary scan test can detect?
Boundary Scan test will be able to diagnose the following failures:

FAQ 2012-12-01

What is SCANSTA112 device?
The SCANSTA112 device is a 7-port multidrop IEEE 1149.1 (JTAG) multiplexer design to connect boundary scan chains into a single chain as well as the ability to remove a board from the system and retain test access to the remaining chains.

FAQ 2012-12-01

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

Why do I need to hold the state of certain pins/nodes?
Non-boundary scan devices such as DDR or flash memories need to hold one or more nodes (chip select/enable) to fixed states during boundary scan testing, so that the device is disabled during boundary scan testing and its output pins (i.e. data) are not activated, as otherwise, it will cause unstable tests or damage to the circuitry. Boundary scan “hold states” are node/device pins on a board that are held to a logic of 1 or 0 by a boundary scan driver on the node, when the boundary scan device driver/output pin is in EXTEST.

FAQ 2012-10-01

What is the CAPTURE State?
During the CAPTURE state, data or instruction bits are loaded in parallel into data or instruction registers. The CAPTURE-DR (Data Register) loads data bits into the specified data register. CAPTURE-IR (Instruction Register) loads instruction bits into the Instruction Register.

FAQ 2012-10-01

XVision fails to install on some laptops
Before installing XVision /ICT software, please follow the steps below:

FAQ 2012-09-25

What is the Boundary Scan device Normal Operation mode?
When the device is operating under the normal mode, the boundary register is transparent. Signals can pass through the boundary scan cells freely and the device operates as it would without test cells. In this mode, test data is captured in the boundary register cells, then shifted through the boundary register out to TDO.

FAQ 2012-09-01

What is the Boundary Scan device Test Operation mode?
During the boundary scan device test operation mode, a single boundary register cell routes input and output signals so the device's core logic essentially ignores the inputs and outputs.

FAQ 2012-09-01

What is Test-Logic-Reset State?
At the test-logic-reset controller state, the test logic is disabled so that normal operation of the boundary scan device can proceed unhindered.

FAQ 2012-08-01

What is Run-Test/Idle State?
The run-test/idle state is a TAP controller state where once entered, the controller state will remain as long as the test mode state (TMS) is held low.

FAQ 2012-08-01

What is a bus wire test?
The bus wire test looks only for opens on all the bussed boundary scan devices that are not tested by the interconnect test.

FAQ 2012-07-01

What is STAPL?
STAPL stands for Standard Test and Programming Language to support programming of programmable logic devices (PLD).

FAQ 2012-07-01

What is IEEE Standard 1581?
The IEEE Standard (Std) 1581 is the standard for Static Component Interconnection Test Protocol and Architecture. The IEEE Std 1581 targets testing for low-cost, complex DDR memory devices, which would be able to communicate through another semiconductor device with an IEEE Std 1149.1 boundary scan capability.

FAQ 2012-06-01

What is IEEE Standard 1149.7?
IEEE Standard (Std) 1149.7 is a standard for reduced-pin and enhanced-functionality test access port (TAP) and boundary scan architecture.

FAQ 2012-06-01

What is Cover-Extend Technology?
Cover-Extend Technology (CET) is a hybrid between VTEP and boundary scan. It draws the best from what each technology offers and enhances the overall capability of Keysight in-circuit test systems.

FAQ 2012-05-01

What are the IEEE standards that are supported or which are being proposed for support by Cover-Extend Technology?
The available IEEE standards/drafts concerning Cover-Extend Technology are IEEE 1149.1 - IEEE Standard Test Access Ports and Boundary Scan Architecture.

FAQ 2012-05-01

What TAP signals are sampled during the rising edge of a TCK signal?
The test mode state (TMS) and test data in (TDI) signals are sampled into the test logic on the rising edge of a test clock (TCK) signal.

FAQ 2012-04-01

What TAP signals are sampled during the falling edge of a TCK signal?
The test data out (TDO) signals of the test access port (TAP) are sampled into the test logic on the falling edge of a test clock (TCK) signal.

FAQ 2012-04-01

How do I determine the maximum test clock (TCK) frequency of the boundary scan device?
The boundary scan device test clock (TCK) information is described in the boundary scan description language (BSDL) at the TAP port identification which assigns a special meaning to these signals.

FAQ 2012-03-01

1 2 3 4 5 6 7 下一页