Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

Categoria de Produto

1-13 de 13

Sort:
Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

How does the Microsoft end of support for Windows XP affect my EXT?
These documents will help you with answers to important questions.

FAQ 2014-05-01

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

When does the BER test apply in the N9081A Bluetooth® measurement application?
The BER test only applies for EDR with a PRBS9 signal pattern.

FAQ 2012-01-10

How do I repair the E6621A measurement application if it fails to launch?
A utility is available that will fix the E6621A measurement application. Click on the question above for a fuller description.

FAQ 2011-12-23

Can I recover the E6621A operating system if it fails to start correctly?
Yes, E6621A has a System Software Recovery mode. Click on the question above for a fuller description.

FAQ 2011-12-21

How do I install the license for my Graphical Measurement Application (GMA) N4017A software?
When you redeem your N4017A entitlement certificate at http:///find/softwarelicense, you must decide if you wish to lock the software to an N4010A test set or to a PC.

FAQ 2010-09-15

Why my N8300A will shut down when I select restart?
The application at N8300A must be close before you restart.

FAQ 2010-03-24

How can I find out when new firmware or software is released?
There are three ways to check for updates.

FAQ 2008-01-09

8920: How Do I Upgrade My Firmware for the 8920A?

FAQ 2002-06-27

Keysight 8920, 8921 Firmware Upgrade Clarification Matrix

FAQ 2002-06-27

8920: How Do I Upgrade My Firmware for the 8920B?

FAQ 2002-06-27