Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 334

Sort:
How do I find the HOST ID of my instrument or PC?
Keysight software options are licensed to many different types of hardware, using a unique hardware identifier called the Host ID. The Host ID is composed of 1, 2, or 3 elements, depending upon the software model and the target hardware platform.

FAQ 2019-07-10

How do I send the UXM Error Logs to Keysight?
You can use the UXM’s Export Logs function to send the UXM platform log files to the Keysight support team. Click on the question for additional information.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Why does my E6640A EXM not have a calibration certificate?
Details can be found here...

FAQ 2017-02-06

How do I upgrade my E6610A Remote Radio Head Tester?
Find Information on upgrade options for the E6610A...

FAQ 2016-02-26

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

Do Y-Applications give me direct connectivity between Signal Studio and my EXM?
Direct connectivity from Signal Studio to the EXM is coming in a future release.

FAQ 2015-02-27

Can Y-Applications and V-Applications co-exist on the same E6640A EXM?
Yes, you may have both Y-Apps and V-Apps on the same EXM.

FAQ 2015-02-27

What is the difference between the V-Applications and the Y-Applications?
The Y-Apps include the ability to run an unlimited number of waveforms for the technology purchased. The V-Apps allow waveform playback based on installation of waveform license “packs” of 5 & 50 licenses.

FAQ 2015-02-27

How do I upgrade my E7515A UXM Wireless Test Set?
Find Information on hardware options available for the UXM.

FAQ 2015-02-05

8960 Test and Lab Application - Annual Contract Subscription
This page provides a single source of test and lab application software downloads for those on the Annual Contract for the 8960 test set (E6720A). If you’re not yet on the Annual Contract and would like to be, contact your local sales representative for details.

FAQ 2015-01-19

How do I upgrade my E6650A EXF Wireless Test Set?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-11-10

Where do I find E6651A Mobile WiMAX™ Test Set Software and Firmware
Links to N64xxA and E665xA software and the neccessary firmware.

FAQ 2014-10-28

Where is my Calibration Certificate for the E6650A EXF?
The E6650A (EXF) does not have a calibration certificate because of its flexible TRX configuration. Only the M9300A Reference and M9440A TRX modules installed inside the E6650A chassis have a calibration certificate

FAQ 2014-09-09

How can the E6650A EXF sequencer help to accelerate my testing speed?
The sequence analyzer is an evolution from traditional measurement method.

FAQ 2014-09-08

Wireless Solutions Software Access
Instructions and downloads for the Wireless Solutions Software: E6965A, E6966A and N5972A

FAQ 2014-08-04

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

How does the Microsoft end of support for Windows XP affect my T1111S and T1212S?
Get the latest information here

FAQ 2014-05-16

HTML HTML
How does the Microsoft end of support for Windows XP affect my EXT?
These documents will help you with answers to important questions.

FAQ 2014-05-01

How do I upgrade my E6640A EXM Wireless Test Set?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-03-06

Why does my USB 3.0 device not work correctly on my E6640A, EXM Wireless Test Set? All my USB 2.0 devices work correctly.
Details about a driver download found here...

FAQ 2014-02-28

How does a user direct a SCPI command to a specific Multi-Port Adapter or to a specific sub-instrument?
Useful commands on how to connect to the X-Host...

FAQ 2013-08-15

How can I get 8960 Lab Application Annual Contract Subscription Release Downloads?
Get the latest downloads here

FAQ 2013-02-28

HTML HTML
Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

How do I get the manuals and release notes for the 8960 (E5515C/E)?
Online User's Guide Index

FAQ 2013-01-18

1 2 3 4 5 6 7 8 9 10 ... Next