Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

Categoria de Produto

1-7 de 7

Sort:
Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.

FAQ 2013-11-17

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

What is EVO and what are the known issues?
EVO is an abbreviation for Extensible VEE Object, which introduce after VEE Pro Version 9.21

FAQ 2011-03-31

IO Libraries Suite: What interfaces and operating systems are supported?
View the Keysight IO Libraries Support matrices.

FAQ 2010-09-08

IO Libraries Suite: What pieces of software do I need to install for the IO Libraries to work?
View the data sheet for the full list of requirements.

FAQ 2010-09-08

Is VEE able to interpret "," as decimal point in Formula box running under German Windows?
No. Please use "." as decimal point as per international standard.

FAQ 2009-11-17

Why did VEE displayed an "out of memory" message even the PC has more than 1GB of memory free after using up only 300MB of memory?
Keysight VEE's could not support such a large memory of usage in a single object or interface.

FAQ 2009-11-08