Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 120

Упорядочить:
Understanding FMCW Automotive Radar
In this application note, we will look at frequency modulated continuous waveform (FMCW) radar technology in detail, particularly the wideband 76-81 GHz range. We will describe how you can use Keysight’s solutions to test your designs to ensure maximum efficiency, reliability, repeatability, and most importantly, ensure that your devices work to the highest safety standards possible.

Руководство по применению 2020-07-23

Latency in Automotive Ethernet Switches
Automotive Ethernet systems rely on speed and timing. Knowing the latency of the overall network is critical. See how to utilize Keysight protocol decode and triggering application to measure the latency in your switch

Руководство по применению 2020-06-18

Automotive Ethernet: Enabling the Future of Autonomous Driving
Autonomous vehicles and advanced driver assistance systems (ADAS) need higher bandwidth and lower latency. Automotive Ethernet is the new backbone for faster onboard networking.

Руководство по применению 2020-03-12

Noise Figure Measurement Accuracy - The Y-Factor Method - Application Note
Specific to instruments that use the Y-factor method for noise figure measurements, this app note discusses measurement basics, avoidable errors, loss and temperature corrections, and uncertainties.

Руководство по применению 2020-03-02

Automotive Serial Bus Testing Using Oscilloscopes - White Paper
Learn how to use oscilloscopes to characterize the performance of your automotive buses including CAN, CAN FD, LIN, FlexRay, and SENT.

Руководство по применению 2019-10-04

Next Generation of Test Automation and Systems - Application Note
Application note covering test automation using PathWave Test Automation Software

Руководство по применению 2019-09-23

PDF PDF 1.06 MB
HP8920 Mode on the M8920A - Application Note
HP8920A to M8920A SCPI Compatibility Mode - BETA Release

Руководство по применению 2019-07-11

PDF PDF 563 KB
Removing Noise in Lithium-Ion Battery Cell Self-Discharge Data Sets
Li-Ion self discharge measurement data shows significant noise, complicating interpretation. This application note presents a series of algorithms that can effectively remove most of this noise, which improves the reliability of cell classification.

Руководство по применению 2019-05-21

Matching Response Times of Lithium-Ion Cell Self-Discharge Current Measurements
New system calibration method assures well-matched response times of self-discharge current measurements, enabling reliable classification of cells more quickly.

Руководство по применению 2019-05-21

USB 2.0 Compliance Testing with Infiniium Oscilloscopes - Application Note
This Application Note discusses the solution for the USB 2.0 test suite. The Keysight solution is the only one-box solution that uses the official USB-IF scripts for precompliance ans compliance testing.

Руководство по применению 2019-01-29

Testing is Critical for Adoption of Autonomous Vehicles - White Paper
The autonomous vehicle combines various connected car technologies such as sensors, computers, and software which need rigorous testing to ensure conformance to safety and performance standards.

Руководство по применению 2018-11-28

Совершенствование систем помощи водителю (ADAS) и беспилотного вождения - Аналитический доклад
Аналитический доклад, посвященный совершенствованию систем помощи водителю (ADAS) и беспилотного вождения с помощью автомобильного радара миллиметрового диапазона.

Руководство по применению 2018-05-29

Testing Automotive DC-DC converter with Keysight TS-8989 - Application Note
This paper discusses emulation of input signals, load simulations and measurements for testing high-power automotive DC-DC converter electronic control units and the TS-8989 functional tester.

Руководство по применению 2018-04-12

PDF PDF 781 KB
Increasing Manufacturing Throughput of Automotive Controllers - Application Note
This application note describes how automotive manufacturers can boost throughput using the Keysight TS-5400 Series 3 high performance PXI function test system for multiple devices under test.

Руководство по применению 2018-02-15

PDF PDF 757 KB
TS-8989 System Integration Guide - Application Note
In today’s manufacturing environment, floor space is an increasingly invaluable variable in the cost of test equation.

Руководство по применению 2017-12-12

PDF PDF 2.69 MB
Measure Lithium Ion Self-Discharge of Cells in a Fraction of the Time Traditionally Required
This new way to determine a cell’s self-discharge by measuring its self-discharge current allows cells with excessively high self-discharge to be identified and isolated much quicker vs traditional open-circuit voltage approaches.

Руководство по применению 2017-12-08

Choosing the Test System Software Architecture - Application Note
This application note is designed to help you quickly design a test system that produces reliable results and meets throughput requirements within budget. It explores the entire software development process, from gathering and documenting software requirements through design reuse considerations.

Руководство по применению 2017-12-05

Accelerating Spurious Emission Measurements Using Fast-Sweep Techniques - Application Note
Searching for spurious emissions can be especially difficult and time-consuming. Learn about techniques you can use to optimize and speed your measurements.

Руководство по применению 2017-12-05

Optimizing Power Product Usage to Speed Design Validation Testing - Application Note
This application note is for design validation engineers who need to conduct complex and/or time-consuming tests using power products. It presents methods and techniques to decrease setup time and test time. It is also useful to the manufacturing engineer, as these methods can be beneficial for manufacturing tests.

Руководство по применению 2017-12-05

Как сократить время тестирования скорости саморазряда литий-ионных элементов питания?–Аналит. доклад
Аналитический доклад, посвященный новому методу тестирования скорости саморазряда литий-ионных элементов питания, который сокращает время, нужное для выявления негодных элементов питания, с нескольких недель до нескольких минут, что позволяет сэкономить средства и ускоряет вывод продуктов на рынок.

Руководство по применению 2017-12-01

6 Hints for Enhancing Measurement Integrity in RF/Microwave Test Systems - Application Note
6 Hints for Enhancing Measurement Integrity in RF/Microwave Test Systems and balancing the tradeoffs between performance, speed, and repeatability.

Руководство по применению 2017-12-01

Right Load Switching and Simulation Design Choices for High Current and Mechatronic Functional Tests
Key considerations for designing a cost-effective high-power switching and load management automotive functional test solution.

Руководство по применению 2017-12-01

PDF PDF 664 KB
The Benefits of Using LXI in Automotive Functional Test
LXI can help maximize performance, minimize cost and extend capital investments into the future. This whitepaper explores the benefits associated with using LXI in Automotive Functional test.

Руководство по применению 2017-12-01

PDF PDF 1.26 MB
Fundamentals of RF and Microwave Noise Figure Measurements - Application Note
This 32-page, black-and-white application note providesinformation on RF and Microwave noise figure measurementts. Topics include noise figure and temperature, noise characteristics of two-port networks, and the measurement of noise figure.

Руководство по применению 2017-09-06

Automotive RF/MW System Verification and Troubleshooting Tests Using FieldFox Handheld Analyzers
This application note discusses the RF and microwave systems in the 21st century car and the challenges to verify their operation and troubleshoot faulty issues.

Руководство по применению 2017-06-21

1 2 3 4 5 Следующие