이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 56

정렬방식:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

신호 및 스펙트럼 분석기 벤치탑/모듈러/핸드형 펌웨어 업데이트 센터
벤치탑 및 핸드형 모델의 신호 및 스펙트럼 분석기용 펌웨어 또는 소프트웨어 최신 버전 액세스.

FAQ 2019-07-11

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

M8000 시리즈를 위한 30일 무료 체험판 라이선스
M8000 제품군 내의 모든 체험판 라이선스에 대한 개요 및 링크

FAQ 2017-01-31

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
PC4 (Dual-Core High Performance Processor) 및 W7X (Window 7 OS) Option을 구매하시면 Window 7으로 upgrade 가능합니다.

FAQ 2014-08-25

How does the Microsoft end of support for Windows XP affect my Keysight AFM or NanoIndenter?

FAQ 2014-05-13

How does the Microsoft end of support for Windows XP affect my EXT?
These documents will help you with answers to important questions.

FAQ 2014-05-01

Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.

FAQ 2013-11-17

Do you have an example C# code to control the N4960A BERT?
Yes.

FAQ 2013-10-21

N5120A 에서 지원하는 CPRI 규격은 어떤 버젼입니까?
N5120A 는 CPRI standard v1.1 까지 지원됩니다.

FAQ 2013-09-27

Do you have an example Python code to control the N4960A BERT?
Yes.

FAQ 2013-09-04

How can I get firmware for the 8614xA/B Optical Spectrum Analyzer?
If your unit needs a firmware upgrade, please contact Keysight Support.

FAQ 2013-09-04

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

Will Windows 7 work on my existing processor?
There is a minimum configuration/vintage of processors which are compatible with Windows 7 and these are denoted as PC4 and PC5 in the show system screen on your instrument

FAQ 2013-04-25

UNH-IOL JBISTGUI Software
JBISTGUI utilizes the two channel mode of J-BERT N4903B and configures transmission of the necessary pattern sequences that can enable the BIST-L and BIST-TAS test modes for SATA host and device products. This Software simplifies Keysight’s receiver test setup by eliminating the need to switch between a protocol tester and J-BERT.

FAQ 2013-03-18

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

How much the default RF port power of N4375B? And can I change it?
It is 0 dBm, and you can change it.

FAQ 2012-03-01

PDF PDF 46 KB
Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

BER 테스트는 N9081A Bluetooth® 측정 어플리케이션에서 언제 적용합니까?
BER 테스트는 PRBS9 신호 패턴과 관련하여 EDR에만 적용됩니다.

FAQ 2012-01-10

How do I repair the E6621A measurement application if it fails to launch?
A utility is available that will fix the E6621A measurement application. Click on the question above for a fuller description.

FAQ 2011-12-23

Can I recover the E6621A operating system if it fails to start correctly?
Yes, E6621A has a System Software Recovery mode. Click on the question above for a fuller description.

FAQ 2011-12-21

1 2 3 다음