検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 58

並べ替え
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-04

ベンチトップ/モジュラー/ハンドヘルドモデルのシグナル・アナライザ/スペクトラム・アナライザのファームウェア・アップデート・センター
ベンチトップ/モジュラー/ハンドヘルドモデルのシグナル/スペクトラム・アナライザのファームウェア/ソフトウェアの最新バージョンを利用するために。

FAQ 2018-05-17

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

M8000シリーズの30日間の無料試用ライセンス
M8000製品シリーズのすべての試用ライセンスへのリンクおよび概要

FAQ 2017-01-30

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

How does the Microsoft end of support for Windows XP affect my Keysight AFM or NanoIndenter?

FAQ 2014-05-13

How does the Microsoft end of support for Windows XP affect my EXT?
These documents will help you with answers to important questions.

FAQ 2014-05-01

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

Does Keysight VEE 9.0 support Windows 7?
Yes. A Keysight VEE patch is currently in development and is tentatively scheduled for release on 2nd quarter of 2010.

FAQ 2013-11-17

N4960A BERTを制御するためのサンプルC#コード

FAQ 2013-11-12

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

How can I get firmware for the 8614xA/B Optical Spectrum Analyzer?
If your unit needs a firmware upgrade, please contact Keysight Support.

FAQ 2013-09-04

Do you have an example Python code to control the N4960A BERT?
Yes.

FAQ 2013-09-04

GPIBインタフェース(82357A、E5810A、82350B)を使って、GPIB経由でPC上から計測器を自動計測する方法を教えてください。
GPIBインタフェース(82357A、E5810A、82350B)を使って....

FAQ 2013-06-19

After purchasing an N9094AK upgrade, must the instrument be sent to a Keysight Service Center to be upgraded?
No. The N9094AK upgrades can easily be installed by the user...

FAQ 2013-04-25

Will Windows 7 work on my existing processor?
There is a minimum configuration/vintage of processors which are compatible with Windows 7 and these are denoted as PC4 and PC5 in the show system screen on your instrument

FAQ 2013-04-25

UNH-IOL JBISTGUI Software
JBISTGUI utilizes the two channel mode of J-BERT N4903B and configures transmission of the necessary pattern sequences that can enable the BIST-L and BIST-TAS test modes for SATA host and device products. This Software simplifies Keysight’s receiver test setup by eliminating the need to switch between a protocol tester and J-BERT.

FAQ 2013-03-18

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

シリアル BERT ソフトウェア
シリアル BERT N4900 シリーズ用の現在のソフトウェアが、そのドキュメントと一緒に用意されています。

FAQ 2012-07-09

N4375BのE/EモードでRFの出力パワーはいくつですか? またその設定を変更できますか?
0dBmに設定されています。 変更する事も可能です。

FAQ 2012-03-01

PDF PDF 56 KB
Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

N9081A Bluetooth®測定アプリケーションでBERテストが適用されるのはいつですか?
BERテストは、PRBS9信号パターンのEDRだけに適用されます。

FAQ 2012-01-22

How do I repair the E6621A measurement application if it fails to launch?
A utility is available that will fix the E6621A measurement application. Click on the question above for a fuller description.

FAQ 2011-12-23

1 2 3 次へ