検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 174

並べ替え
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

IO Libraries Suite: Can the IO Libraries be installed as a silent install?
Yes. The install can be silent with the correct command line parameters.

FAQ 2014-04-07

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

Keysight VEEはノートPCで使えますか?
はい、使用できます。

FAQ 2013-11-17

Keysight VEE は旧バージョンとの互換性がありますか?
基本的には、旧バージョンのVEEで作ったプログラムファイルをLOAD, RUNさせることは可能です。

FAQ 2013-11-17

[操作方法] PCから、オシロをWebブラウザ/LAN経由で遠隔コントロールするには、どのようにすれば良いでしょうか?
弊社のオシロスコープ(InfiniiVision、Infiniium)には、Webコントロール機能が内蔵されており、遠隔地からLANを経由してリモート制御する事が可能になっています。

FAQ 2013-10-28

E8257D PSGアナログ信号発生器のアップグレード
ハードウェア・アップグレード、測定器ソフトウェアに関する情報の検索

FAQ 2013-08-20

複数の34945EXTを接続するためのRJ45制御ケーブルの最大全長は?
RJ45制御ケーブルの全長(最大)は約42.7 mです。

FAQ 2013-05-13

Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

86100C/86100Dデジタル・コミュニケーション・アナライザの消費電力の代表値は?
86100C/86100Dの代表的な測定の消費電力

FAQ 2012-09-25

What can I do if I fail to establish hardware connection after successfully installing Keysight USB modular instrument driver on a Win7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

[仕様] 5485x/DSO80000/90000AシリーズのBNCコネクタは、高帯域でも使用できるのでしょうか?
5485x、DSO80000、DSO90000AシリーズInfiniiumオシロスコープは「プレシジョンBNC」コネクタを使用しています。

FAQ 2012-05-09

8167シリーズ/8168シリーズの波長可変レーザ光源(8167A/B, 8168A/B/C/D/E/F)で、コネクタ・オプション021、022、023の違いは ?
一般的なフラット・フィジカル・コンタクト出力です。光コネクタ・インタフェースによって特定のコネクタ・タイプが決まります。

FAQ 2012-02-17

Keysight 8761B SPDT同軸スイッチが『Keysight 34945A/L4445A/L4490A/L4491A構成ガイド』に記載されていません。その理由は?
8761Bの内部デザインで、コイルの制御端子間のDC極性の反転によってRF経路が選択されるためです。Keysight 34945A/L4445A/L4490A/L4491A制御ユニットは、極性反転モードを備えていません。このため、8761Bは、34945A/L4445A/L4490A/L4491A制御ユニットでは制御できません。

FAQ 2012-01-30

ENAアナライザとSCPI-LANで通信するためHP Basicを設定する際の情報はありますか?
ENAのLAN設定を認識するためにHP Basic AUTOSTを設定します。

FAQ 2011-10-07

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

What are the minimum system requirements for i3070 TDW?

FAQ 2011-03-02

ENAおよびE5092Aの測定セットアップ用のアクセサリ(ケーブルやアダプタ)を入手する方法は?
RFセミリジッド・ケーブルやアダプタなどの、テスト・セットアップ用のアクセサリは、E5092A拡張可能マルチポート・テスト・セットのオプションに含まれています。テスト・セットに接続するE5071C ENAネットワーク・アナライザのオプションに応じて、適切なアクセサリのセットを選択できます。

FAQ 2011-01-27

How do I install N7700A packages on a computer/instrument like the N7788BD without internet access?
This can easily be done by copying the neccessary download files from another computer with internet access...

FAQ 2010-10-18

[操作方法] ユーザ名とパスワードを入力せずにInfiniiumオシロスコープを使用するには?
デフォルト設定では、マシンに搭載されているWindows 95/98、Windows XPオペレーティング・システムはユーザ名とパスワードを使ってログインする必要があります。

FAQ 2010-10-06

1 2 3 4 5 6 7 次へ