이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

226-250 / 1746

정렬방식:
What is a compliance enable pin?
Compliance enable pins must be held with stable logic states as described in the boundary scan description language (BSDL) before the device can be engaged in any 1149.1 boundary scan activities.

FAQ 2011-11-01

How to access board directories resided on the Linux/Unix server using SAMBA/Common Internet File System (CIFS), if ICT controller is on Windows® 7?
SAMBA is a utility which allows you to share your files between Linux/UNIX and Windows®. By mounting the SAMBA share on your Linux/UNIX server, you can access the board files across the operating systems.

FAQ 2011-11-01

How can I set up File Security and board directories with NFS share?
Once you have enabled “Client for NFS”, you can mount any NFS share on your network. There are a few ways to set up NFS share file security.

FAQ 2011-11-01

How can I access my i3070/3070 ICT board directories residing on Linux/UNIX controller, if I am running my ICT controller on Windows® 7?
Services for Network File System (NFS) and Subsystem for UNIX-based Applications (SUA) are the software packages provided by Microsoft® to enable the UNIX subsystem and other parts of the UNIX environment to be integrated onto the Windows environment.

FAQ 2011-11-01

What is a USERCODE instruction?
The USERCODE is an optional instruction in the boundary scan description language) (BSDL) that allows a 32-bit user programmable identification code to be loaded and shifted out for examination.

FAQ 2011-11-01

What are the known conflicts between MKS NutCracker and Interix and the recommended workaround solutions?
There are three known key issues which you need to look out for:

FAQ 2011-11-01

이전에 구매한 스코프/로직애널라이저의 소프트웨어 라이선스를 다시 설치할 수 있나요?
주문번호와 certificate 번호가 필요합니다.

FAQ 2011-10-23

85033E 30kHz~9GHz 교정 키트 위상의 어댑터가 일치합니까?
예.

FAQ 2011-10-07

SCPI-LAN을 통해 키사이트 ENA 분석기와 통신하기 위해 HP Basic을 구성하는 아웃라인이 있습니까?

FAQ 2011-10-07

85039B F형 교정 키트의 delay/thru 정의에 오류가 있습니까?

FAQ 2011-10-07

키사이트 제품용 액세서리는 어디에서 구할 수 있습니까?
기기별 액세서리(오실로스코프용 프로브 등)가 필요한 경우 우선 제품 페이지로 가서 관련 액세서리를 살펴 보십시오. 범용 액세서리(rf 및 마이크로웨이브 테스트 액세서리, 카트 및 랙 등)가 필요한 경우에는 테스트 및 측정 액세서리, 캐비닛 및 케이블 페이지로 가면 됩니다.

FAQ 2011-10-07

What is “Device Identification Register”?
Use of the optional device identification register allows a data to be serially read from the device.

FAQ 2011-09-27

What is “Boundary Length"?
The “Boundary Length” defines the number (length) of cells in the boundary scan register.

FAQ 2011-09-27

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

What is the shielding type used by Keysight GPIB cable?
Keysight GPIB cable is double shielded standard cable

FAQ 2011-09-12

Windows® 7 for i3070 system and controller upgrade
Effective October 22, 2011 all new i3070 systems and PC controller upgrades will be pre-installed with Microsoft Windows 7 operating system.

FAQ 2011-09-04

What is a boundary scan chain?
A boundary scan chain consists of two or more boundary scan devices

FAQ 2011-08-29

What are the Keysight Medalist i3070 limited access test solutions?
Traditional in-circuit test (ICT) techniques are based on the assumption of 100% electrical test access to nodes on a printed circuit board assembly (PCBA). However...

FAQ 2011-08-29

Eight commonly asked questions about the Medalist i3070 Series 5
The i3070 Series 5 sports various innovative hardware and software features to bring you much wider test coverage and superb throughput for cost savings and faster time to profit. Check out these key features.

FAQ 2011-08-08

What is a CPLD ISP?
The Keysight Medalist ICT system can be used to program IEEE 1149.1 compliant CPLD using the test access port (TAP). This programming becomes part of the overall testplan and is executed during in circuit test (ICT).

FAQ 2011-07-29

What is a silicon nail test on Keysight Medalist i3070?
The silicon nail test refers to the use of boundary register cells to replace the needs for physical probes on nodes during in circuit testing of non boundary scan device.

FAQ 2011-07-29

Does Keysight offer an LC adapter for modules?
Keysight Technologies offers different ways to connect an LC connector to our optical instrumentation.

FAQ 2011-07-08

What accessories should I order with a 8163X power sensor module?
The power sensors will not be able to operate as standalone instruments.

FAQ 2011-07-06

What accessories should I order with the 816XX Tunable Laser Sources?
See long answer.

FAQ 2011-07-06

Can I use APC connectors with the 8163x optical power sensor modules?
Yes, you can use the optical power sensors with straight (PC) or angled (APC) fiber at the input.

FAQ 2011-07-06

이전 1 2 3 4 5 6 7 8 9 10 ... 다음