検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

151-175 / 2051

並べ替え
What is the performance difference between the N8212A module with Option 016 and the N8241A arbitrary waveform generator synthetic instrument module?
The N8212A with Option 016 is based on the E8267D PSG signal generator with Option 016; the N8241A is based on the N6030A arbitrary waveform generator.

FAQ 2012-12-28

VEE Pro: Where can I find information on Keysight VEE Pro Panel Drivers?
VEE Pro Panel Drivers are available from the Drivers, Firmware, and Software section of the VEE product page...

FAQ 2012-12-18

WireScope™ Pro Software Download

FAQ 2012-12-18

Where do I get Java to display the 34980A web interface?
The Java Virtual Machine code is needed to run the Keysight 34980A web page features. A free download of the Java Virtual Machine (JVM) can be obtained by going to the following web site.

FAQ 2012-12-17

Can I remotely query the 86100D DCA-X to determine which user interface is running?
Yes. Issue the query :SYSTem:FCONfig? If the response is "Legacy" then the legacy UI is in use. If the response is "Compatible" or "Standard" then the FlexDCA interface is in use.

FAQ 2012-12-12

N490xA/BシリアルBERTを使用して、所定の信頼性レベルでビット・エラー・レート(BER)を測定するには?
デジタル伝送システムの品質を決定する方法の 1つとして、ビット・エラー・レート(BER)の測定があります。

FAQ 2012-12-11

9.953Gb/sのデータレートで10-12のBERを測定するのにどのくらいの時間がかかりますか? 2.488Gb/sの場合はどうですか?
いつエラーが発生するかと言う事を正確に予測することは不可能です。したがって、確率統計から求められるConfidence Level を使用して、10-12より優れたBER性能を備えていると言えるだけの長い期間にわたってエラーなくテストする必要があります。

FAQ 2012-12-11

10 MHz基準入力/出力を備えているKeysightオシロスコープは?
6000シリーズ、6000Lシリーズ、7000Aシリーズ、7000Bシリーズ、9000シリーズ、54850シリーズ(出力のみ)、80000Aシリーズ、80000Bシリーズ、90000Aシリーズ、90000 Xシリーズ

FAQ 2012-12-10

What is SCANSTA112 device?
The SCANSTA112 device is a 7-port multidrop IEEE 1149.1 (JTAG) multiplexer design to connect boundary scan chains into a single chain as well as the ability to remove a board from the system and retain test access to the remaining chains.

FAQ 2012-12-01

What are the failures that boundary scan test can detect?
Boundary Scan test will be able to diagnose the following failures:

FAQ 2012-12-01

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

Why are some of the features shown in the Framescope user manual not available in software version 7.0.5?
Users might encounter different features when using Framescope software version 7.0.5 versus what is stated in the documentation.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

外部ミキサ・オプションEXMは、11974シリーズ プリセレクト・ミキサをサポートしますか?
11974シリーズ プリセレクト・ミキサをN9030A PXAでサポートする予定はありません。

FAQ 2012-10-25

導波管フランジ用の交換用保護キャップを注文するには?
下記の表をご参照下さい。

FAQ 2012-10-23

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

How to report a VEE bug, serious error or submit an enhancement request effectively?
1. Go to the VEE Help menu and select Customer Feedback option...

FAQ 2012-10-16

FrameScope Pro Download

FAQ 2012-10-16

所有するPXAで使用できる外部ミキサは?その注文方法は?
現在、オプションEXM付きPXAは、11970シリーズ(11970Kを除く)またはOML Inc.(旧Oleson Microwave Lab)社のミキサと組み合わせて使用できます。

FAQ 2012-10-15

IO Libraries Suite: Can I use VXI on a 64-bit OS?
IO Libraries Suite 16.1 (or later) supports VXI (E8491A/B and E1406A) on 64-bit Vista, 7, Server 2008 R2...

FAQ 2012-10-10

IO ライブラリ・スイート:IO モニタとは?
IO モニタは、Keysight VISA、VISA COM、SICL IO ライブラリの I/O コールをトレースするユーティリティです。

FAQ 2012-10-09

IO ライブラリ・スイート:付属のスイート 14以降で以前のバージョンを使用できますか?
Keysight の測定器を 1台お持ちのお客様には、バージョンに関係なく、IO ライブラリの 1つのライセンスを使用する法的権利があります。

FAQ 2012-10-08

IO ライブラリ・スイート 15.0 ライセンスが付属していますか?
Keysight では、約 150種類のKeysight の測定器モデル、GPIB および I/O コンバータ製品.....

FAQ 2012-10-08

Why do I need to hold the state of certain pins/nodes?
Non-boundary scan devices such as DDR or flash memories need to hold one or more nodes (chip select/enable) to fixed states during boundary scan testing, so that the device is disabled during boundary scan testing and its output pins (i.e. data) are not activated, as otherwise, it will cause unstable tests or damage to the circuitry. Boundary scan “hold states” are node/device pins on a board that are held to a logic of 1 or 0 by a boundary scan driver on the node, when the boundary scan device driver/output pin is in EXTEST.

FAQ 2012-10-01

前へ 1 2 3 4 5 6 7 8 9 10 ... 次へ