技术支持
缩小范围
按主题
- 校准 (30)
- 配置和安装 (158)
- 显示信息和误差代码 (33)
- 许可 (12)
- 测量和仪器的基础知识 (50)
- 测量技术 (90)
- 操作系统和软件 (56)
- 操作和功能 (218)
- 其它信息 (56)
- 部件和附件 (68)
- 打印和打印机 (10)
- 产品与固化软件更新及升级 (50)
- 产品操作原理 (61)
- 编程和数据传输 (129)
- 服务和维护 (77)
- 规范和精度 (76)
- 故障诊断 (28)
行业/技术
按内容类型
- FAQ (1732)
按产品类别
1-25 / 1732
Is there a 3D model of the Infiniium 9000 Series oscilloscope?
Yes, see the Step format file download.
FAQ 2019-11-04 |
|
Signal & Spectrum Analyzer Benchtop/Modular/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.
FAQ 2019-10-30 |
|
Which version of Visual Studio is working with TestExec SL?
Which version of Visual Studio will work with TestExec SL ?
FAQ 2019-10-08 |
|
Does Test Exec SL software support backward compatibility?
Can Test Plan Created on TestExec SL 8.1 can run on TestExec SL 7.1?
FAQ 2019-10-08 |
|
What version of TS-5000 is working with TestExec SL?
Which version of TS-5000 will work with TestExec SL 8.1?
FAQ 2019-10-08 |
|
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.
FAQ 2019-08-28 |
|
M8000 系列的 30 天免费试用许可证
M8000 产品系列的所有试用许可证的简介和链接。
FAQ 2019-04-16 |
|
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
FAQ 2018-12-10 |
|
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FAQ 2018-12-10 |
|
Does Keysight offer teaching courseware on Industry 4.0 and IoT?
Keysight U380xA IoT Applied Courseware series offers a ready-to-teach package that includes hands-on industry relevant experiences and real-world applications such as Smart Home, Smart City, Smart Automobile and Industry 4.0. Click to find out more.
FAQ 2018-10-25 |
|
为 200GAUI-4 和 400GAUI-8 C2M 接收机测试设置推荐的仪器配置
为 200GAUI-4 和 400GAUI-8 C2M 接收机测试设置推荐的仪器配置(附件未列出)
FAQ 2018-08-20 |
|
What upgrade options are needed to update my Windows operating system, processor board or solid state drive on my X-Series signal analyzer?
Details about X-Series signal analyzer operation system, processor and solid state drive dependencies
FAQ 2018-08-13 |
|
x6000 End of Support
End of Support - x6000 Automated X-Ray Inspection system
FAQ 2018-08-07 |
|
How do I remove the root login password on the U3800A Intel Edison?
If the password is misplaced or lost, you will need to reflash Intel Edison firmware. Otherwise, you can remove the password from Edison’s system file.
FAQ 2018-07-25 |
|
How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts
FAQ 2018-02-26 |
|
IO Libraries Suite: What is the latest version? IO Libraries Suite 2018 Update 0.2
IO Libraries Suite 2018 Update 0.2, available online.
FAQ 2018-01-31 |
|
How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.
FAQ 2017-12-14 |
|
Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF.
Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states.
If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly.
To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF.
Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.
FAQ 2017-11-13 |
|
Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA
FAQ 2017-09-21 |
|
What are the recommended power supplies used for U9391C/F/G?
Power supply
FAQ 2017-08-07 |
|
Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.
FAQ 2017-07-28 |
|
What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.
FAQ 2017-07-13 |
|
How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.
FAQ 2017-06-28 |
|
How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.
FAQ 2017-06-28 |
|
How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.
FAQ 2017-06-28 |
|