您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Designing Custom Filters using Direct Synthesis and Network Transforms Webcast

1   小時 | 網路廣播 -- 存檔 | 地點與時間

INNOVATIONS IN EDA

WHY THIS WEBCAST IS IMPORTANT

Unlike designing filters using template scaling of known topologies, direct synthesis starts from designing the custom filter response, followed by synthesizing all possible filter topologies from the customized filter transfer function. You then select the topology that is most economical and convenient for realization. Additional network transforms are then applied to the chosen topology for practical implementation into lumped and/or distributed circuits. Learn how to use this powerful direct synthesis technique for the design of custom filters, diplexers and matching networks from examples in a new book titled Filter Synthesis presented by the author.

WHO SHOULD ATTEND

RF, Microwave and Analog circuit or system designers who need to implement custom filter response such as notches, diplexers and multiplexers for their applications.

PRESENTER

Randy Rhea, Founder, Eagleware / Elanix Corporation

Randy Rhea graduated at the University of Illinois (69) and Arizona State (73), and worked at the Boeing Company, Goodyear Aerospace and Scientific-Atlanta. He founded Eagleware Corporation and Noble Publishing, which were acquired by Keysight Technologies in 2005 and by SciTech Publishing in 2006, respectively. He has authored numerous papers and four books, and has taught workshops to over a thousand engineers worldwide at symposium, companies and the Georgia Institute of Technology. He is retired and resides with his wife of 44 years in an antebellum plantation home near Thomasville, Georgia. 

地點與時間

費用 地點 詳細資訊
免費 At Your PC Enroll to view the June 26, 2014 recorded broadcast 

上表所列為參考訂價,如有任何變更,恕不另行通知。