Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Multi-antenna Array Measurements Using Digitizers Webcast

1   Hour | Интернет-трансляция - записи | Где и когда

WHAT IS THE WEBCAST ABOUT

There are numerous applications that employ antenna arrays for beamforming. From commercial and satellite communications to radio astronomy and RADAR, multiple antennas are employed for spatial selectivity and interference avoidance through beamforming techniques. When designing a phased array for beamforming, it is important to be able to measure the relative phase and amplitude between antennas in the array while minimizing errors caused by phase offsets created in the test system. For example in a dynamic phased array, the adjustable phase shifters in each element “steer” the antenna and therefore need to have known phase relationship by the control system that is used to point the beam in the desired direction. The better the cross-channel phase coherence is of the measurement system used to align the antennas, the more precisely the beam can be positioned.

This webcast will discuss using a multi-channel phase coherent digitizer, along with the necessary signal conditioning and down-conversion ahead of the digitizer, to characterize the relative phase and amplitude relationships between antennas in a phased array. The discussion will cover: calibrating a digitizer-based system for matched cross-channel magnitude and phase, using digital down-conversion for optimizing the system sensitivity at the required bandwidth, and algorithms used on the resulting complex signals necessary to achieve measurement results of cross-channel (between antennas) phase and gain. At the conclusion of the paper, a representative system configuration will be described with measurement results derived from the techniques presented.

WHO SHOULD ATTEND

This webcast will be of interest to systems and test engineers that develop and evaluate antenna systems for radar or communications uses. Particularly those working in the area of multiple antenna and phased array beamforming systems should attend. Additionally, it will be useful for engineering managers that need more information on new measurement technologies and their affect on the cost of testing these antenna systems.

PRESENTER

Alexander Dickson, Application Engineer, Agilent Technologies

Alex is an Application Engineer working for Agilent Technologies in Loveland, CO. Alex joined Agilent Technologies in July 2000 as a college hire and has worked in a variety application engineering and marketing positions. His background in instrument automation and oscilloscopes led to his most recent opportunity to work within Keysight’s growing modular instrument division. In his spare time he enjoys running and biking the recreational trails around Loveland.

Ссылки по теме

Где и когда

Стоимость Место проведения Подробнее
Бесплатно At Your PC Enroll now for the May 29, 2013 recorded broadcast 

Приведены цены из прайс-листа. Цены могут меняться без уведомления.

Материалы семинаров и тренингов

Multi-antenna Array Measurements Using Digitizers Webcast Slides 
Slides from the may 29, 2013 webcast

Материалы семинаров 2013-05-29

PDF PDF 1.35 MB