Electronics & Applications 2017
Tradeshow | Where & When
Visit Keysight at stand D041 at Electronics & Applications 2017 in Utrecht, The Netherlands from May 30th to June 1st.
Held in Jaarbeurs Utrecht, Hall 7, it will host the complete branches of industrial electronics from the Benelux. More than 130 companies will exhibit for three days, promoting their innovations, knowledge and skills in industrial electronics. Representatives from the clusters design & engineering, electronic components, test & measurement and electronics production exhibit at the fair.
In addition to the exhibition a complete conference program is provided. This program consists of nine seminars that focus on the current developments in electronics.