Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

What is BenchVue 2017 software?

BenchVue 2017 is an introduction of enhanced BenchVue apps as well as new BenchVue apps that allow you to control your test instruments and simplify your test processes. Each BenchVue app includes:

  • Instrument control with no programming needed.
  • Data visualization for data logs and other measurements.
  • Test automation using BenchVue Test Flow to build automated tests as easily as using your instrument front panel saving you days to months of data collecting time or test development.
  • Easy data exports to formats such as .CSV, Microsoft Word, Excel, or MATLAB.

What instruments does BenchVue 2017 work with?

Currently, BenchVue software is enabled on over 470 Keysight instruments. Please visit www.keysight.com/find/BenchVueInstruments for the latest list of supported Keysight instruments.

Do I need to pay for BenchVue 2017? My current version is free

  • The BenchVue platform software, required to run the BenchVue apps, is still provided at no-cost.
  • Most of the BenchVue 2017 apps require a paid license for use. To determine if your app requires a paid license, visit the web page for your particular app to find out licensing details. BenchVue offers flexible licensing options starting at less than $100 USD. A free 30-day license can also be enabled directly from the App Tab in BenchVue Once you have installed BenchVue 2017 and your desired app(s), simply navigate to your app’s details page within the App Tab and press the Start Trial button. A complete list of BenchVue apps can be found at www.keysight.com/find/BenchVue_Apps
  • Nearly all BenchVue 2017 licensed apps now include use of Test Flow enabling you to easily build automated test sequences without requiring instrument programming such as the use of SCPI or IVI commands.
  • You can download the new BenchVue 2017 apps via the App Tab in the BenchVue platform software or visit: www.keysight.com/find/BenchVue_Apps

Can I go back to my older version after installing BenchVue 2017?

Yes. First uninstall BenchVue 2017, then download the older version you would like to install. You will need to have the installers for the older versions of your apps in order to downgrade. Use the Apps tab in the older version of BenchVue to download and install your app.

Why should I upgrade to the 2017 version of my BenchVue apps?

Starting with this version of the BenchVue apps, we are including Test Flow automation with all app models that end with a “B”. Test Flow enables you to easily build automated test sequences without requiring instrument programming such as the use of SCPI or IVI commands.

Example, the BenchVue Digital Multimeter app is now called the “BV0001B BenchVue Digital Multimeter Control & Automation app” and includes Test Flow.

Upgrading to the 2017 versions of BenchVue apps ensures you have all of the latest features and advancements for all of your apps. Your new license includes free updates for 1 year.

What’s a Control and Automation App?

The BenchVue Control and Automation apps include the ability to easily connect to your instruments, control them without programming, and perform some basic analysis such as visualized data logging. These apps also include controls and measurements that have the ability to be automated in our Test Flow workspace. Simply drag the orange box controls into the workspace. With BenchVue 2017, test automation can now be executed as simply as using your instrument’s front panel allowing every engineer to easily create automated tests. For more information on Test Flow visit www.keysight.com/find/BenchVueTestFlow

What’s a Control and Analysis App?

The BenchVue Control and Analysis apps include the ability to easily connect to your instruments, control them without programming, and perform more in depth analysis with better data visualization than the Control and Automation apps. These apps include more instrument controls and faster data acquisition rates that have been optimized for measurements. These apps do not yet have the built-in Test Flow controls, but Test Flow may be used for automation via SCPI blocks or Command Expert blocks.

  • BenchVue Data Acquisition App (BV0006B) is a Control and Analysis App.
  • BenchVue Power Meter/Sensor App (BV0007B) is a Control and Analysis App.

Can I migrate only certain applications?

No. In order to migrate to BenchVue 2017, the BenchVue platform software and all previous versions of BenchVue apps need to be upgraded.

How can I get a license?

  • A free 30-day license is available via the Apps tab in BenchVue. Once you have the BenchVue platform software installed, simply install your BenchVue app, navigate to your app’s details page within the App Tab and press the Start Trial button.
  • You may also purchase BenchVue 2017 apps directly from Keysight via a Keysight representative or from one of our Keysight Sales Partners.

Can I have BenchVue 2017 and an older version installed simultaneously?

No, you can only have one version of BenchVue installed on your PC.

How much does an application cost?

  • BenchVue has flexible licensing options for every budget and a variety of use cases. Prices start at <$100 USD. For more specific price information, visit the individual app pages for quick quotes www.keysight.com/find/benchvue  or contact Keysight or your local Keysight sales partner.
  • One license enables one PC for usage.
  • BenchVue also has a Complete Control Collection (BV9001B) that is a collection of BenchVue 2017 apps. Purchasing this collection will ensure that nearly all your Keysight instrument types will be supported when you use BenchVue. To see what’s included in the this collection visit www.keysight.com/find/BenchVueCCC

Will I lose all my data if I migrate to BenchVue 2017?

No, upgrading to BenchVue 2017 will not delete your data. Your previous data logs will be preserved in the Data Manager.

How can I get help or report bugs for BenchVue software? 

Please visit: www.keysight.com/find/contactexpert_BV

Request additional BenchVue instrument support or additional features? 

Please send email: benchvue.feedback@keysight.com