Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discuter avec un expert

In N7625B, how many instances of carriers and carrier aggregations do the software support?

One connected signal generator can support one instance of Carrier Aggregation mode.

One instance of Carrier Aggregation can support 5 component carriers.

The Carrier Aggregation mode (whether configured for 1 component carrier or for the maximum of 5 carriers) still counts as 1 carrier of the 16 carrier maximum.