Sample program files: E5061B ENA Custom Multiport Switch Solution using L4491A (5990-9359EN)
Overview:
This is the sample VBA program and the switch configuration file which is referred in the application note "Design Tutorial: E5061B ENA Custom Multiport Switch Solution using L4491A" (5990-9359EN).
How to install and run this file:
Copy the download .vba and .csv file to the D:\VBA folder of your E5061B. To run the macro, press [Macro Setup] on the E5061B front panel, then select Load & Run, and click on "MultiportControl_E5061B_xxxx" on the softkey menu.
文件及下載
MultiportControl_E5061B_0100.vba
程式編寫範例 2011-10-24 |
![]() |
SW_Config_E5061B.csv
程式編寫範例 2011-10-24 |
![]() |
Design Tutorial: E5061B ENA Custom Multiport Switch Solution Using L4491A
This application note describes how to configure a 12-port custom switch box with the L4491A switch platform and operation basics using the E5061B network analyzer.
應用手冊 2011-11-29 |
![]() |