이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

WLAN Virtual Front Panel

The WLAN Virtual Front Panel software is one example of a remote interface for controlling the N4010A Wireless Connectivity Test Set. It is an application provided free with the N4010A hardware and is ideally suited for bench-top testing of an 802.11a/b/g/n WLAN device. Commonly it is used for characterization of devices in accordance with 802.11 specifications. The application is a good tool for familiarization of tests before full production tests are written and customised using the N4010A WLAN driver (DLL). The N4010A WLAN driver is an Application Programming Interface (API) which can be used for custom test development. The WLAN Virtual Front Panel application uses the N4010A WLAN driver as a demonstration of what can be achieved by integrating the driver into a software environment. The driver can be used in any programming environment that supports Microsoft® .NET or COM.

Microsoft is a U.S. registered trademark of Microsoft Corporation.