Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

What signal sources are support for use as an alignment source for the PSA / N9039A RF Preselector based system?

A list of supported signal sources can be found in the PSA by pressing Mode Setup, Config EMI Receiver, Source Config, Model Number while in the EMC Analyzer mode. These currently are:

  • 8648B
  • N5181A
  • N5182A1
  • N5183A2,3
  • N5161A2
  • N5162A2
  • E4438C
  • E8257D3

While others may be added in the future, these are the only sources currently supported.

1 With PSA firmware version A.11.01 and newer
2 With PSA firmware version A.11.08 and newer
3 Option 1E1 Required