这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

What signal sources are support for use as an alignment source for the PSA / N9039A RF Preselector based system?

A list of supported signal sources can be found in the PSA by pressing Mode Setup, Config EMI Receiver, Source Config, Model Number while in the EMC Analyzer mode. These currently are:

  • 8648B
  • N5181A
  • N5182A1
  • N5183A2,3
  • N5161A2
  • N5162A2
  • E4438C
  • E8257D3

While others may be added in the future, these are the only sources currently supported.

1 With PSA firmware version A.11.01 and newer
2 With PSA firmware version A.11.08 and newer
3 Option 1E1 Required