Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Is it possible to reset the 8970A,B Noise Figure Instrument Storage/Recall States to Factory Defaults?

Follow the Instructions below to reconfigure the Noise Figure Meter Storage states to factory default conditions.

1. Press 0.9 - Special Function followed by the green PRESET key (this will recall and initialize all Special Function settings and reset the current state).

2.Press STORE 0, STORE 1, STORE 2,..., STORE 9 (this will store the default factory settings to the 10 internal registers of the Noise Figure Meter).

Note that this has NO EFFECT on the ENR storage tables. See separate FAQtitled "How to Reset the 8970A,B ENR Table Entries to Default"