Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

B1500A Application Test : Timing On-The-Fly NBTI Test Method

Library Installation:

Install this software update in the following instrument.

  • B1500A with EasyEXPERT

Import this application test definition into the EasyEXPERT Library.

The initial release of "NBTI(Id)" application test definition is imported in the new "NBTI" library category.

The second release of "NBTI(Id)_2" application test definition is imported in the new "NBTI" library category.

Revision:

This application test definition runs on EasyEXPERT A.02.10 or later.

Documentation:

Refer to the application note in Documents and Downloads below.

Timing on-the-fly NBTI(Id) 2.zip file includes a readme for the second release features.

Documents & Downloads

Timing On-the-Fly NBTI(Id) 
Initial release application test definition.

Programming Example 2006-10-10

Timing On-the-Fly NBTI(Id) 2 
Second release application test definition.

Programming Example 2007-02-22

AN B1500A-6 Accurate NBTI Characterization Using Timing-on-the-Fly Sampling Mode 
This four-page application note details how the B1500A and Keysight's timing-on-the-fly NBTI test method solves many of the problems associated with traditional NBTI test methods.

Application Note 2006-10-01