Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

What is the performance difference between the N8212A module with Option 016 and the N8241A arbitrary waveform generator synthetic instrument module?

The N8212A with Option 016 is a synthetic instrument based on the E8267D PSG signal generator with Option H16. It does not have a display or an internal Arb.

The N8241A is a synthetic instrument based on the N6030A arbitrary waveform generator. Communication with the N8241A is made through LAN, not an NI interface.