Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

What is the equivalent command to "Output after Sweep" parameter on "Sweep" dialog?

The SCPI command equivalent to the parameter "Output after Sweep" in the "Sweep" dialog which can be shown by pressing
>>Config>Source>Sweep
function keys should be [:SOURce]:FUNCtion:TRIGgered:CONTinuous.
Once you send it with the parameter "ON", the parameter is set to "END VALUE".