Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Can I set the different limit values for each of polarities on the B2961A/B2962A?

The B2961A/62A has the capability to set not only single V/I Limit but also V/I Limit for Each Polarity. In the default setting, the same limit values are used for both positive and negative polarities. Once V/I Limit for Each Polarity is enabled, the instrument can have the different limit value for each of polarities.

Please see the following material for the details.
How to select V/I Limit setup operation on B2961A/B2962A