Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Is it possible to change the font size of softkey menu on ENA?

(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)

Yes. The font size of softkey menu can be changed with following procedure.

  1. [System] > [Misc Setup] > [Display Setup] > [Magnification]
  2. Select [Large], [Normal], or [Small]

 

Font Size - Small

Fig1. [Small] Magnification

 

Font Size - Normal

Fig2. [Normal] Magnification

 

Font Size - Large

Fig3. [Large] Magnification