您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

E5080B Network Analyzer Firmware Software Revision History

Additions/Changes for Version A.14.10.13 . . . (compiled Sep 26, 2020)
• (Bug Fix) Response Tracking correction data is incorrect at high gain setting.
• (Bug Fix) CALC:MEAS:MARK:DIST works correctly in query but not for setting.

Additions/Changes for Version A.14.10.12 . . . (compiled Aug 25, 2020)
• (Bug Fix) Crash on saving the citifile on the Differential IQ channel
• (Bug Fix) Crash during ECal with averaging in remote.
• (Bug Fix) Group Delay Aperture softkey causes crash if no trace.
• (Bug Fix) File reading failed error on Cal Pod recorrect
• (Bug Fix) SA application locks up after a trace is deleted and a new trace is added

Additions/Changes for Version A.14.10.08 . . . (compiled July 31, 2020)
• Support S96089B Differential and I/Q devices measurements
• Support Data Viewer
• (Bug Fix) System calibration for receiver compression at HIGH gain works wrongly.
• (Bug Fix) Adding new channel in advanced mode breaks TDR stimulus setting
• (Bug Fix) TDR causes error at start-up when DIF1/DIF2
• (Bug Fix) FOM softkey cannot be enabled
• (Bug Fix) NF Fixture Turn On Crash with non-default port setting
• (Bug Fix) TDR Auto DUT length does not work correctly
• (Bug Fix) Waveform does not change after the parameter change with CALC:FSIM:BAL:PAR:BBAL:DEF
• (Bug Fix) (Bug Fix) Cal All cannot run Ecal vector cal without doing a power sensor calibration
 

Additions/Changes for Version A.14.10.03 . . . (compiled Apr 15, 2020)

• Support Multiport Calibration Assistant
• Support S9xxxxB application software for floating/USB portable licenses.
• Fixed Gain Cal
• Support Cal Pods
• Support U205xXA/U206xXA Series USB Power Sensors.
• Support the following items in the spectrum analysis.
      • Noise Power Ratio (NPI) measurement
      • Coherent Averaging Tab
      • Pulsed SA (Trigger & Pulse Tab, Pulse settings in source Tab)
      • Dual Band Configuration in advance tab
      • SA analysis marker

Additions/Changes for Version A.13.90.15 . . . (compiled Apr 09, 2020)
• (Bug Fix) "Execution error" occurs when performing Response Cal, 2port THRU.
• (Bug Fix) USB Power Sensor doesn't work with A.13.90.06.

Additions/Changes for Version A.13.90.09 … (compiled Dec 18, 2019)
Minor bug fixes
 

Additions/Changes for Version A.13.90.07 . . . (compiled Nov 21, 2019)
New: Supports S9x083A Vector and Scalar Mixer/Converter Measurements
Several bug fixes
 

Additions/Changes for Version A.13.90.06 . . . (compiled Sep 5, 2019)
New: Supports the frequency up to 53 GHz (options 2L0, 2M0,2N0, 2P0, 4L0, 4M0, 4N0, 4P0)
New: Supports the second source (options 442, 462, 492, 4D2, 4H2, 4K2, 4L2, 4M2, 4N2, 4P2)
New: Device Expert
New: Source Power Alignment tool
New: PLL Bandwidth selection for better phase noise (command only)
New: List-sweep mode in trigger mode for external source

Firmware Revision A.13.70.02 … Released May 2019
Initial release