您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Command Expert 2019 Release Notes

About Command Expert
 

Keysight's Command Expert software combines instrument commands, documentation, syntax checking, command execution, and code generation all in one simple interface. Command Expert works with instruments that use Standard Commands for Programmable Instrumentation (SCPI), IVI-C,  IVI-COM, or IVI.NET drivers.

Command Expert generates a SCPI.NET driver for each SCPI command set you install, for use in Visual Studio applications.

Command Expert Add-ons let you use Command Expert for easy instrument control in Excel, LabVIEW, MATLAB, Python, SystemVue, VEE, and Visual Studio.
 

What's In Command Expert 2019

Adds support for the following environments

  • Python 3.7
  • LabView 2018
  • MATLAB 2018b
  • MATLAB 2019a
  • Excel 2019
  • Visual Studio 2019

Other changes and features

  • Fixed Keysight VISA being installed as Primary VISA.
  • Corrected the overwrite of primary VISA with visa32.dll.
  • Command Expert now successfully supports the add-on arbitrary data type.
     

Supported Instruments

To see which SCPI instruments are supported, use the Manage Command Sets dialog box in the Command Expert application, or visit Instruments Supported by Command Expert

Command Expert also lets you control instruments using IVI-COM, IVI-C, and IVI.NET drivers.

 

 Last Updated: March 9, 2019