您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

How do I upgrade my N9041B UXA Signal Analyzer?

Most all of the UXA options that are sold at the time of instrument purchase are also available as an upgrade option. The upgrade contents are listed in the tables below as Hardware, Software, License Key, or some combination of the three.  Hardware retrofit kits will contain the assemblies to be installed as well as the installation instructions.  In many cases a license key will be required to activate the hardware option or measurement application.

Upgrade options are categorized as:

  • Internal Hardware Upgrades (Ex. Preamplifier or 40 MHz Analysis Bandwidth)
  • External Hardware Upgrades (Ex. Rackmount Kit or Minimum Loss Pad)
  • Instrument Software (Ex. Instrument Software Download File or Measurement Applications)

Internal Hardware Upgrades:

Before a hardware upgrade is purchased from Keysight the following steps should be taken:

  1. Go to the "Installed By" column and read the installed by defininition.
  2. View the installation note if available by selecting the "Install Note" links in the tables below for the desired upgrade option.
  3. Determine from the Installed By definition and the installation note the complexity of the installation and whether you will perform the upgrade yourself or have a Keysight Service Center do it for you.
  4. Review the Utilities, Adjustments & Performance Verification Tests section of the installation note to see what the required adjustments and performance tests are once the upgrade is installed.
  5. Review the following lists of test equipment requirements for each required adjustment and performance test to further determine whether you have the ability to perform the upgrade yourself or have an Keysight Service Center do it for you.
  • UXA Adjustments (Not Available)
  • UXA Performance Verification Tests (Not Available)

If an upgrade option is going to be installed by a Keysight Service Center, additional labor charges will apply. Your Keysight field engineer can provide an all inclusive quote for this.

All instrument adjustments are automated and require the use of the Keysight Performance Verification & Adjustment Software (Not Available)

Many hardware upgrades will require the redemption and installation of a license key file (.lic) to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website

N9041B Internal Hardware Option Upgrades
Option Description Order As eDelivery Upgrade Contents Minimum Firmware Adjustments Required1 Additional Requirements Incompatible With Installed By Installation Time
ALV Auxiliary Log Video Out

N9041BU-ALV
 

Yes
  1. Install Note
  2. Entitlement Certificate
None No None None Advanced User1

Install=0.5 Hrs
Adjust & Verification=0.5 Hrs

B40 Increase Analysis Bandwidth from 25 MHz to 40 MHz N9041BU-B40 Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No None None User1

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

CRP
Add Arbitrary I.F. Output N9041BU-CRP Yes
  1. Install Note
  2. Entitlement Certificate
None No None None Advanced User1 Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
CRW IF Out, Wide (Rear Panel Connector) N9041BU-CRW Yes
  1. Install Note
  2. Entitlement Certificate 
None  No 

None

None  User Install = 0.5 Hrs
Adjust & Verify = 0.5 Hrs.
 
EA3 Add Electronic Attenuator to 3.6 GHz N9041BU-EA3 Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No None None User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs  
EDC External Digitizer Control N9041BU-EDC Yes
  1. Install Note
  2.  Entitlement Certificate
A.21.00 No Option CRW None User Install=0.5 Hrs
Adjust & Verify=0.0 Hrs
 
EMC Add Precompliance EMI Features N9041BU-EMC Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No None None User Install=0.5 Hrs 
Adjust & Verify=0.5 Hrs 
F22 Frequency Range Upgrade from 90 GHz to 110 GHz N9041BU-F22 No
  1. Hardware
  2. Entitlement Certificate
None Yes Option 590 5CX Factory Only Not Available at this time
FBP Full Bypass Path N9041BU-FBP No Factory will provide licensing, adjustment and verification A.23.14 Yes Option H1G Instruments that do not have Option H1G Factory Only Install=0.5 Hrs
Adjust & Verify=20 Hrs
 
FP2 Fast Power N9041BU-FP2 Yes
  1. Install Note (Coming soon)
  2. Entitlement Certificate
None No Option B40 None User Install=0.5 Hrs Adjust & Verify=0.5 Hrs
FT1 Frequency Mask Trigger, basic detection N9041BU-FT1 Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No Option H1G None User Install=0.5 Hrs Adjust & Verify=0.5 Hrs
FT2 Frequency Mask Trigger, optimum detection N9041BU-FT2 Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No Option H1G None User Install=0.5 Hrs Adjust & Verify=0.0 Hrs
H1G Increase Analysis Bandwidth from 25 or 40 MHz to 1 GHz  N9041BU-H1G No
  1. Hardware
  2. Entitlement Certificate
A.19.17 Yes None None Factory Only

Not Available at this time

P50 Add Preamplifier, 50 GHz N9041BU-P50 Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No None None User1

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

RT1

Add Real-time Spectrum Analyzer up to Maximum Analysis Bandwidth

-Basic Detection

N9041BU-RT1

Yes
  1. Install Note
  2. Entitlement Certificate
None No Option H1G None User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
RT2

Add Real-time Spectrum Analyzer up to Maximum Analysis Bandwidth

-Optimum Detection

N9041BU-RT2 Yes
  1. Install Note
  2. Entitlement Certificate
None No Option H1G None User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
SF1 Add Security Features, Exclude Launch Programs N9041BU-SF1 Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No None None User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
SF2 Add Security Features, Prohibit Saving Results N9041BU-SF2 Yes
  1. Install Note
  2. Entitlement Certificate
None No None None User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
SSD Additional Removable Solid State Drive N9041BU-SSD No
  1. Hardware
  2. Install Note
None No None None User

Install=1.0 Hrs
Adjust & Verify=0.0 Hrs

W10 Windows 10 Solid State Drive ⇒MUST READ N9041BU-SS1 No
  1. Hardware
  2. Install Note
  3. Software
None No2 PC6 None Advanced User Install=1.0 Hrs
Adjust & Verify=0.0 Hrs
 
YAV Add Y-axis Video Output N9041BU-YAV Yes
  1. Install Note (Coming Soon)
  2. Entitlement Certificate
None No None None User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

1Upgrade can be performed by the User without any performance verification required if the instrument being upgraded is still within it's factory calibration cycle. See the upgrade installation note for more details.

N9041B External Hardware Option Upgrades
Option Description Order As eDelivery Installation Note Upgrade Contents Minimum Firmware Adjustments Required Additional Requirements Incompatible With Installed By Installation Time
DVR USB DVD-ROM/CD-R/RW Drive 1DVR001A No None Hardware None None None None Not applicable Not applicable
KB2 Compact Keyboard 1KBD001A No None Hardware None None None None Not applicable Not applicable
MLP Minimum Loss Pad, 50 to 75 Ohms MLP001A No None Hardware None None None None Not applicable Not applicable
MSE USB Mouse

1MSE001A

No None Hardware None None None None Not applicable Not applicable
2CM Rackmount Kit w/o Handles N9041BU-2CM No None Hardware None None None None Not applicable Not applicable
2CP Rackmount Kit w/Handles N9041BU-2CP No None Hardware None None None None Not applicable Not applicable

Instrument Software

Instrument Software Update:

The software update package for the UXA Signal Analyzer contains the spectrum analyzer measurement application, all the advanced measurement application software, and all other updates required by the individual measurement assemblies inside the instrument.

Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the analyzer.

The latest revision of the instrument software installer can be found at:

Measurement Applications:

To see the complete list of software measurement applications available for the N9041B Signal Analyzer see:

Measurement Applications require the redemption and installation of a license key file (.lic). Measurement application upgrades are meant to be performed by the end user customer, and no adjustments or performance verification tests are required.

In order to redeem a license key, the end user customer must have a valid redemption certificate and then go to the Keysight Software License Redemption Website

Available Accessories:
 

文件及下載

如何將頻譜 / 信號分析儀升級? 
執行頻譜分析儀或信號分析儀升級的資訊。

常見問題 2014-12-18