您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

[E5063A Sample Program] Save Trace Data Macro

Overview

This sample program enables the E5063A ENA user to save the multiple channel/trace data with various formats. This is an executable file and the source code is not disclosed.

Revision Number

Rev.01.01

Supported functions

  • Data save as Active trace only, Active channel all traces, Displayed channel and all traces

  • CSV, MATLAB, and CITI format saving

  • Corrected or formatted data and memory saving

How to register and execute this macro

  • Registering the macro

1. Copy the download file to your ENA.
2. Press [Macro Setup] on the ENA front panel and select Macro Setup ….
3. In the Macro Title box, type a descriptive title for the macro.
4. Click Browse, and select the download file.
5. Click OK.

  • Executing the macro

1. Press [Macro Menu].
2. Select the name of this macro, then press [Enter].

Macro Image
 

文件及下載

SaveTraceDataForE5063A_0101.exe 

程式編寫範例 2015-05-20

null EXE 742 KB
Manual_SaveTraceDataForE5063A.pdf 

使用手冊 2015-05-20

null PDF 300 KB