您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

N5182A MXG RF Vector Signal Generator Upgrades

Upgrade LogoPlease Note: The information provided on this page is for reference only. The upgrades for these products are no longer available.

 

Hardware upgrade kits contain installation instructions and the desired assembly. Adjustments or performance verifications may be required to ensure the instrument meets the published specifications.

  • Some performance verification tests can be performed using the N7800A Calibration & Adjustment Software. All adjustments must be performed using the N7800A Calibration & Adjustment Software.
  • More involved upgrades require the instrument be shipped to a Keysight Service Center to have the upgrade installed. Make sure to obtain a quote for the installation before sending the instrument and upgrade kit to a Keysight Service Center to get installed. A full calibration is the only way to guarantee specifications are being met.

The table below provides an Installation Note for each upgrade. The installation note includes a list of the performance verification tests and adjustments required as well as the test equipment and test software necessary to complete the upgrade. In most cases the instrument will need to be sent to a Keysight Service Center.

Hardware upgrades may require that a minimum firmware is already installed. Up-to-date firmware can be downloaded for free from the MXG Firmware Upgrade Center.

Some hardware upgrades may also require the redemption and installation of a license key before they will be activated. Once a redemption certificate is received, the license key(s) can be redeemed at the Software License Redemption Website

Option Description Order As Installation Note Upgrade Contents Minimum Firmware Adjustments Required Additional Requirements Incompatible With Installed By - Estimated Time
006 Instrument security N5182AK-006 License key installation Software, License key > A.01.04 None None None Customer - 0.5 Hrs
012 LO in/out for phase coherency N5182AK-012 Available Hardware, License key > A.01.42 None None None Customer - 1.0 Hrs
019 Increase baseband generator memory to 64 MSa N5182AK-019 License key installation Software, License key > A.01.04 None 651 or 652 or 654 None Customer - 0.5 Hrs
099 Expanded license key upgradeability N5182AK-099  Available Hardware, License key > A.01.42 Suggested verification test1 None None Customer - 1.5 Hrs
1EA High power N5182AK-1EA License key installation Software, License key > A.01.42 None 099 None Customer - 0.5 Hrs
1EL Differential I/Q outputs N5182AK-1EL License key installation Software, License key > A.01.04 None 651 or 652 or 654 None Customer - 0.5 Hrs
1EQ Low power (< -110 dBm) N5182AK-1EQ License key installation Software, License key > A.01.42 None 099 None Customer - 0.5 Hrs
1ER Flexible reference input (1-50 MHz) N5182AK-1ER License key installation Software, License key > A.01.04 None None None Customer - 0.5 Hrs
221-229 Waveform License 5-Pack N5182AK-221  License key installation Software, License key > A.01.20 None None None Customer - 0.5 Hrs
250-259 Waveform License 50-pack N5182AK-250 License key installation Software, License key > A.01.50 None None None Customer - 0.5 Hrs
320 Pulse Train Generator N5182AK-320 License key installation Software, License key > A.01.65 None UNU or UNW or HNS None Customer - 0.5 Hrs
403 Calibrated AWGN N5182AK-403 License key installation Software, License key > A.01.04 None 651 or 652 or 654 None Customer - 0.5 Hrs
430 Multitone and two tone N5182AK-430 License key installation Software, License key > A.01.20 None 651 or 652 or 654 None Customer - 0.5 Hrs
431 Custom digital modulation N5182AK-431 License key installation Software, License key > A.01.20 None 651 or 652 or 654 None Customer - 0.5 Hrs
432 Phase noise impairment N5182AK-432 License key installation Software, License key > A.01.20 None 651 or 652 or 654 None Customer - 0.5 Hrs
503 Frequency range options Only available at time of instrument purchase Not applicable Not applicable Not applicable Not applicable Not applicable  Not applicable Not applicable
506
651 Internal baseband generator (30 MSa/s, 8 MSa) N5182AK-651 License key installation Software, License key > A.01.04 None None None Customer - 0.5 Hrs
652 Internal baseband generator (60 MSa/s, 8 MSa) N5182AK-652 License key installation Software, License key > A.01.04 None None None Customer - 0.5 Hrs
654 Internal baseband generator (125 MSa/s, 8 MSa) N5182AK-654 License key installation Software, License key > A.01.04 None None None Customer - 0.5 Hrs
670 Upgrade baseband generator from 30 MSa/sec to 60 MSa/sec N5182AK-670 License key installation Software, License key > A.01.20 None 651 None Customer - 0.5 Hrs
671 Upgrade baseband generator from 30 MSa/sec to 125 MSa/sec N5182AK-671 License key installation Software, License key > A.01.20 None 651 None Customer - 0.5 Hrs
672 Upgrade baseband generator from 60 MSa/sec to 125 MSa/sec N5182AK-672 License key installation Software, License key > A.01.20 None 652 None Customer - 0.5 Hrs
ALB LXI compliant functionality N5182AK-ALB License key installation Software, License key > A.01.51 None None None Customer - 0.5 Hrs
R2C Revision to current, core instrument FW enhancements N5182AK-R2C License key installation Software, License key > A.01.60 None None  None  Customer - 0.5 Hrs
UNT AM, FM, phase modulation N5182AK-UNT License key installation Software, License key > A.01.42 None 099 None Customer - 0.5 Hrs
UNU Pulse modulation N5182AK-UNU License key installation Software, License key > A.01.42 None 099 UNW Customer - 0.5 Hrs

UNV

 

Enhanced dynamic range N5182AK-UNV License key installation Software, License key > A.01.42 None 099 None Customer - 0.5 Hrs

UNW

Narrow pulse modulation N5182AK-UNW License key installation Software, License key > A.01.42 None 099 None Customer - 0.5 Hrs
UNZ Fast switching N5182AK-UNZ License key installation Software, License key > A.01.42 None 099 None Customer - 0.5 Hrs

 

N5182A Accessories
Option Description Order As Installation Note Upgrade Contents Minimum Firmware Adjustments Required Additional Requirements Incompatible With Installed By - Estimated Time
1CM Rack mount kit N5182A-1CM  None Hardware  None None None 1CN, 1CP, 1CR Customer - 1.0 Hrs
1CN Front handle kit N5182A-1CN  None Hardware None None None 1CM, 1CP Customer - 1.0 Hrs
1CP Rackmount and front handle kit N5182A-1CP None Hardware None None None 1CM, 1CN, 1CR Customer - 1.0 Hrs
1CR Rack slide kit N5182A-1CR None Hardware None None None 1CM, 1CP Customer - 1.0 Hrs
AB1 Printed copy of MXG family user's guide - Korean localization N5182A-AB12 None User's guide None None None None Not applicable
AB2 Printed copy of MXG family user's guide - Chinese localization N5182A-AB22 None User's guide None None None None Not applicable
ABA Printed copy of MXG family English documentation set N5182A-ABA None Documentation set None None None None Not applicable
ABJ Printed copy of MXG family user's guide - Japanese localization N5182A-ABJ2 None User's guide None None None None Not applicable
AKT Printed copy of MXG family user's guide - Russian localization N5182A-AKT2 None User's guide None None None None Not applicable
AXT Hard transit case N5182A-AXT None Hardware None None None None Not applicable
CD1 CD-ROM containing the English documentation set N5182A-CD1 None Documentation set None None None None Not applicable

1 Post repair verification test may require one or more of the following equipment: power meter, power sensor, spectrum analyzer, and frequency counter. Verification test time included in repair time estimation.

2 Refer to the MXG family English documentation (N5182A-ABA) for the most current information.

文件及下載

Signal Generator Firmware Update Center 
Download signal generator firmware, release notes, upgrade guide and FAQs.

常見問題 2019-07-19