您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

Can I use the Quick Print button to quickly save my waveforms into the USB thumbdrive?

Yes, but with Keysight InfiniiVision 5000/6000/7000 Series oscilloscope software version 5.10 and above you have to enable the feature:

  1. Make sure you have the latest firmware for the oscilloscope (version 5.10 and above). See: InfiniiVision 5000/6000/7000 Series Oscilloscope Software
  2. Press the Save/Recall key on your oscilloscope. Then, press the Quick Print softkey to enable the feature.
  3. Press the Save softkey, then the Format softkey, to select the format.
  4. Plug in your USB thumbdrive.
  5. Acquire a waveform; then, press the Quick Print key (or Print key on the 7000 Series oscilloscope) to quickly save your waveform.

相關連結