Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

How can I turn on the Services for NFS on Windows® 7 ICT controller?

Both the Windows 7 Ultimate and Windows Enterprise Edition contain the client for the Network File System (NFS) and Subsystem for UNIX-based Applications (SUA). These are the software packages provided by Microsoft® to enable the UNIX subsystem and other parts of the UNIX environment onto Windows environment. However, please note that SUA or Service for UNIX (SFU) will be discontinued in Windows 8.

Turning on Services for NFS

On either Windows 7 Ultimate or Windows Enterprise OS, Services for NFS are turned off by default. You can turn on these services as follows: Access Control Panel → Programs → Programs and Features → Turn Windows features on or off (see figure below).

If you are mapping NFS share only, click on “Services for NFS” including “Administrative Tools” and “Client for NFS” (see figure below):

Related FAQs:


1. How can I access my i3070/3070 ICT board directories residing on Linux/UNIX controller, if I am running my ICT controller on Windows® 7?

2. How can I turn on the SUA and its UNIX utility package on Windows® 7 ICT controller?

3. How can I set up File Security and board directories with NFS share?

4. How can I access board directories residing on the Linux/UNIX controller using SAMBA, if my ICT controller is on Windows® 7? 

5. What are the known conflicts between MKS NutCracker and Interix and the recommended workaround solutions?

*Microsoft and Windows are trademarks or registered trademarks of Microsoft Corporation in the United States and/or other countries.