Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Which printers are supported by the handheld oscilloscopes?

Keysight handheld oscilloscopes will work with printers from major manufacturers which offer native support PCL6, 5e,5c and Postscript level 3 emulation printer command languages. Please note that some printers such as LaserPro type printer is not compatible with our oscilloscopes. The data sheet for each individual printer will identify the printer command language(s) supported by the printer. This statement is not an endorsement or preference for any specific vendor’s product.