Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Does the ENA-L support a built-in web page similar to the 871x family?

The ENA-L units that were shipped with the firmware revision 2.0 and later have a built-in web page server (web-enabled control) capability.

Special Note
Web-enabled control function and user recovery function are NOT provided by firmware upgrade. These functions are available when the volume label on the hard disk is AL200 or higher (for the ENA-L shipped after September 2005). If the volume label on the hard disk is AL100, it's necessary to replace a hard disk with the latest at the service center in order to make this function available.

The ENA-L is the direct replacement for 871x family of vector network analyzers. For additional information on the ENA-L visit https://www.keysight.com/find/ena